Part Number: PROCESSOR-SDK-AM62X
Other Parts Discussed in Thread: SK-AM62
Hi All,
I am working on,
1.AM62xx processor EVM (SK-AM62)
2. AM62xx processor custom board
For above using below requirements
1. JTAG (XDS110 JTAG debug probe)
2. CCS 12.3.0 (Code Composer Studio)
Trying to do "JTAG Interface testing", while doing this test, unable to detect the device and giving the below error
*************************************************************************************************
[Start: Texas Instruments XDS110 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\<user >\AppData\Local\TEXASI~1\
CCS\ccs1230\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100/110/510 class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Mar 10 2023'.
The library build time was '17:27:27'.
The library package version is '9.11.0.00128'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.
The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.
[End: Texas Instruments XDS110 USB Debug Probe_0]
********************************************************************************************************
reference link following from TI,
AM62x MCU+ SDK: Getting Started
Please let me know any suggestions.
regards,
Padmalatha