Other Parts Discussed in Thread: OMAP-L137
Are there any example GEL files floating around for the c6747?
thanks,
-howy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L137
Are there any example GEL files floating around for the c6747?
thanks,
-howy
You can get it from the spectrum digital site (DSP Gel File):
http://support.spectrumdigital.com/boards/evmomapl137/
The full software package can be obtained at:
The C6747 and OMAP-L137 share the same Starter Kit which contains an OMAP-L137 processor (TI Orderable as TMDXOSKL137BET). Note that the OMAP-L137 and C6747 are the same device except the C6747 does not include the ARM9 core.
If interested in evaluating only the C6747 DSP core and not the OMAP-L137 DSP+ARM capabilities simply ignore the ARM core and configure CCS to communicate with the C6747 board.