This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks Akshay,
soon i will mail you the yuv data.
There is no specific scenarion for which this problem occurs, we observed while camera running, at some time the decoding is not happening, then you stored the live data
and found this is the problem.
Akshay ,
it is not possible to capture the yuv data of the particular stream at a point as you are aware of this problem happens at some partcular time while camera running.
i will provide you the camera setting parameters while this kind of problem is happening.
if you want to analyse the the MJPEG encoded stream then i have already attached it in my 1st message, which you can play in VLC player.
Akshay,
i got the following details from SQE when they observed the same problem.
1. Configuration - 1:
- Resolution 1920x1080
- FPS 10
- Compression - 10
- Max bitrate 10240
1. Configuration - 2:
- Resolution 2048x1536
- FPS 10
- Compression - 10
- Max bitrate 10240
Sujit,
I'm unable to reproduce this scenario at my end to enable debugging.
Examining the code also does not yield any clues as to why this behaviour would be occurring. Are there any other details you could share with us that might perhaps give a better insight?
Regards,
Akshay