Hello.
I am working with the TI AAC CODEC on a DM6467 under Montavista Linux 2.6.18. When I capture a file I am not able to play it back. mplayer and VLC reports multiple errors. I have checked the raw PCM preceding it and it is OK. Also, when I stream it out with RTSP/RTP I can hear it OK with VLC. As far as I can see there is a problem with the header information or the specific encoding is confusing to the player. Can anyone help me out here? Attached is the file.
Michael Stamler