Other Parts Discussed in Thread: CCSTUDIO
I am starting to setup the PINMUX registers for the 6747 and I have not found any header files defining their locations.
I have also searched all *.h files (in c:\CCStudio_v3.3\*.*) for "CHIP_6747" and have not found any which makes me think I am missing something.
I have the register locations by the way, I just might be a bit confused as to what components I need to add to CCS to support the 6747.
I have CCS v3.381.6
codegen v6.1.8
DSP BIOS 5.33.03
Is there anything else I need to properly support a DSP BIOS application for the 6747?
thanks,
-howy