This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: TI Ethernet/IP linux

Part Number: AM4376

Hello,

I wan to start Ethernet/IP development for TI Linux AM4376 part.

I have installed PRU-ICSS-Ethernet/ip_Adapter-01.00.03.04 linux version.

do i need to generate project using 

https://software-dl.ti.com/processor-industrial-sw/esd/docs/indsw/ethernetIP_adapter/01_00_03/PRU_ICSS_EthernetIP.html#generating-project-files

and do i need to have linux SDK installed? if yer which version is required?

and also suggest if patches mentioned in getting started are applicable to linux SDK version (which is required to EIP work.)?  

regards,

Vrund