OMAP3 processors have HDMI output, which is very nice. I was wondering, however, if it would be possible to use the HDMI port for video input. It seems that no one has done it yet.
I would like to use my OMAP3530-based Gumstix Overo board to read live video from a HD camera, such as the Contour+ ( http://www.bikerumor.com/2011/05/13/contour-gets-official-with-hdmi-out-microphone-in-wider-angles/ ). Is the hardware capable, provided that I write drivers for it?