Part Number: TDA4VM
Hi,
I try to run vision_apps in SBL boot flow with combined_appImage on j721e. The mcu1_0 app seems working,but Linux can’t boot sucessfully.
Thanks.
The logs:
NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 22:56:45, Mar 3 2023
ERROR: GTC_CNTFID0 is 0! Assuming 200000000 Hz. Fix Bootloader
I/TC:
I/TC: OP-TEE version: 3.20.0 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Fri Mar 3 22:59:24 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
I/TC: HUK Initialized
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 sa2ul_init:59 Failed to get SA2UL device
E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x00063c20 failed
I/TC: Primary CPU switching to normal world boot
E/TC:0 0
E/TC:0 0 Core data-abort at address 0x10 (translation fault)
E/TC:0 0 esr 0x96000005 ttbr0 0x9e894000 ttbr1 0x00000000 cidr 0x0
E/TC:0 0 cpu #0 cpsr 0x800003c4
E/TC:0 0 x0 000000009e867000 x1 0000000000000010
E/TC:0 0 x2 0000000000000000 x3 0000000000000000
E/TC:0 0 x4 0000000000000001 x5 0000000000ffffff
E/TC:0 0 x6 0000000000000002 x7 000000009e89c190
E/TC:0 0 x8 000000009e89c190 x9 000000009e884d70
E/TC:0 0 x10 0000000000000000 x11 0000000000000000
E/TC:0 0 x12 000000009e89c100 x13 000000000000000a
E/TC:0 0 x14 00000000ffffffff x15 0000000000000020
E/TC:0 0 x16 000000009e813c40 x17 0000000000000000
E/TC:0 0 x18 0000000000000000 x19 000000009e89eca0
E/TC:0 0 x20 000000009e89eca8 x21 0000000000000007
E/TC:0 0 x22 000000009e873000 x23 000000009e8736a0
E/TC:0 0 x24 0000000100000000 x25 0000000000000000
E/TC:0 0 x26 0000000000000000 x27 0000000000000000
E/TC:0 0 x28 0000000000000000 x29 000000009e89ec30
E/TC:0 0 x30 000000009e80e3ac elr 000000009e80e3cc
E/TC:0 0 sp_el0 000000009e89ec30
E/TC:0 0 TEE load address @ 0x9e800000
E/TC:0 0 Call stack:
E/TC:0 0 0x9e80e3cc
E/TC:0 0 Panic 'unhandled pageable abort' at core/arch/arm/kernel/abort.c:572 <abort_handler>
E/TC:0 0 TEE load address @ 0x9e800000
E/TC:0 0 Call stack:
E/TC:0 0 0x9e8087dc
E/TC:0 0 0x9e81506c
E/TC:0 0 0x9e807fd8
E/TC:0 0 0x9e805520