Hi Al
I have benn build up th mcu1_0, and out-> vx_app_rtos_linux_mcu1_0.out already exist.
I change the uboot and /lib/firmware/j721s2-main-r5f0_0-fw.
check the process that mcu1_0 seems not runing .
I also change the uboot, still the same.
k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work
1064128 bytes read in 12 ms (84.6 MiB/s)
Load Remote Processor 2 with data@addr=0x82000000 1064128 bytes: Success!
425420 bytes read in 9 ms (45.1 MiB/s)
Load Remote Processor 3 with data@addr=0x82000000 425420 bytes: Success!
199632 bytes read in 8 ms (23.8 MiB/s)
Load Remote Processor 4 with data@addr=0x82000000 199632 bytes: Success!
187344 bytes read in 7 ms (25.5 MiB/s)
Load Remote Processor 5 with data@addr=0x82000000 187344 bytes: Success!
14946336 bytes read in 85 ms (167.7 MiB/s)
Load Remote Processor 6 with data@addr=0x82000000 14946336 bytes: Success!
10489864 bytes read in 61 ms (164 MiB/s)
Load Remote Processor 7 with data@addr=0x82000000 10489864 bytes: Success!
What's the next step?
Did I missed somethings?
Thanks for your help.
Best Regards,
Ming Lu