Part Number: AM623
Other Parts Discussed in Thread: SK-AM62
Setup: Default Version 09.00.00.03 SDK Image booting from SDCARD on SK-AM62 EVM and Digilent Pcam5 OV5640 Image sensor. Device Overlay for camera is loaded via u-boot.
I wish to unload/load the camera driver module ov5640.ko - which isn't possible (says module in use) unless the j721e_csi2rx is unloaded first.
rmmod j721e_csi2rx
rmmod ov5640
insmod /lib/modules/6.1.33-g40c32565ca/kernel/drivers/media/i2c/ov5640.ko
insmod /lib/modules/6.1.33-g40c32565ca/kernel/drivers/media/platform/ti/j721e-csi2rx/j721e-csi2rx.ko
Is there some other camera related modules that should be unloaded/loaded. Is there a specific order this needs to be done in? It doesn't seem to happen on the first unload/load, only the second attempt.
These are the crashes, whch sometimes vary:
****
Nothing - complete lock up of the UART console
*****
[ 189.858267] ti-sci 44043000.system-controller: Mbox timedout in resp(caller: sci_clk_determine_rate+0x64/0xe4)
[ 189.868325] ti-sci 44043000.system-controller: Mbox send fail -110
[ 189.874528] ti-sci-clk 44043000.system-controller:clock-controller: determine-rate failed for dev=135, clk=0, ret=-110
[ 190.914251] ti-sci 44043000.system-controller: Mbox timedout in resp(caller: sci_clk_determine_rate+0x64/0xe4)
[ 190.924278] ti-sci 44043000.system-controller: Mbox send fail -110
[ 190.930464] ti-sci-clk 44043000.system-controller:clock-controller: determine-rate failed for dev=135, clk=0, ret=-110
[ 191.970250] ti-sci 44043000.system-controller: Mbox timedout in resp(caller: sci_clk_determine_rate+0x64/0xe4)
[ 191.980272] ti-sci 44043000.system-controller: Mbox send fail -110
[ 191.986457] ti-sci-clk 44043000.system-controller:clock-controller: determine-rate failed for dev=135, clk=0, ret=-110
[ 191.997151] cpu cpu0: _opp_config_clk_single: failed to set clock rate: -22
[ 192.004115] cpufreq: __target_index: Failed to change cpu frequency: -22
[ 193.026261] ti-sci 44043000.system-controller: Mbox timedout in resp(caller: sci_clk_determine_rate+0x64/0xe4)
[ 193.036291] ti-sci 44043000.system-controller: Mbox send fail -110
[ 193.042476] ti-sci-clk 44043000.system-controller:clock-controller: determine-rate failed for dev=135, clk=0, ret=-110
[ 194.082251] ti-sci 44043000.system-controller: Mbox timedout in resp(caller: sci_clk_determine_rate+0x64/0xe4)
[ 194.092272] ti-sci 44043000.system-controller: Mbox send fail -110
[ 194.098456] ti-sci-clk 44043000.system-controller:clock-controller: determine-rate failed for dev=135, clk=0, ret=-110
[ 195.138250] ti-sci 44043000.system-controller: Mbox timedout in resp(caller: sci_clk_determine_rate+0x64/0xe4)
[ 195.148270] ti-sci 44043000.system-controller: Mbox send fail -110
[ 195.154459] ti-sci-clk 44043000.system-controller:clock-controller: determine-rate failed for dev=135, clk=0, ret=-110
[ 195.165152] cpu cpu0: _opp_config_clk_single: failed to set clock rate: -22
[ 195.172114] cpufreq: __target_index: Failed to change cpu frequency: -22
*****
[ 2735.658621] ti-sci 44043000.system-controller: Mbox timedout in resp(caller: ti_sci_cmd_put_device+0x18/0x24)
[ 2735.668611] ti-sci 44043000.system-controller: Mbox send fail -110
[ 2755.246589] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 2755.252707] rcu: 0-...0: (1 GPs behind) idle=5d4c/1/0x4000000000000000 softirq=44506/44507 fqs=1049
[ 2755.261833] rcu: 2-...0: (2 GPs behind) idle=c36c/1/0x4000000000000000 softirq=35186/35187 fqs=1049
[ 2755.270956] rcu: 3-...0: (8 ticks this GP) idle=6a24/1/0x4000000000000000 softirq=46240/46241 fqs=1049
[ 2755.280338] rcu: Tasks blocked on level-0 rcu_node (CPUs 0-3): P143/1:b..l
[ 2755.287305] (detected by 1, t=5252 jiffies, g=102293, q=105 ncpus=4)
[ 2755.293735] Task dump for CPU 0:
[ 2755.296955] task:insmod state:R running task stack:0 pid:6448 ppid:5487 flags:0x00000206
[ 2755.306863] Call trace:
[ 2755.309304] __switch_to+0xe4/0x160
[ 2755.312807] lock_timer_base+0x64/0xa4
[ 2755.316557] del_timer_sync+0x4c/0xd0
[ 2755.320215] schedule_timeout+0x88/0xf0
[ 2755.324051] wait_for_completion_timeout+0x74/0x144
[ 2755.328925] tx_tick+0x44/0xa4
[ 2755.331982] Task dump for CPU 2:
[ 2755.335200] task:systemd-udevd state:R running task stack:0 pid:194 ppid:1 flags:0x00000a02
[ 2755.345106] Call trace:
[ 2755.347544] __switch_to+0xe4/0x160
[ 2755.351030] 0xffff000004abb900
[ 2755.354168] Task dump for CPU 3:
[ 2755.357386] task:kworker/3:1H state:R running task stack:0 pid:137 ppid:2 flags:0x0000000a
[ 2755.367295] Workqueue: kblockd blk_mq_run_work_fn
[ 2755.372000] Call trace:
[ 2755.374438] __switch_to+0xe4/0x160
[ 2755.377924] __blk_mq_run_hw_queue+0x80/0xbc
[ 2755.382189] blk_mq_run_work_fn+0x20/0x30
[ 2755.386194] process_one_work+0x1d0/0x320
[ 2755.390199] worker_thread+0x14c/0x444
[ 2755.393942] kthread+0x10c/0x110
[ 2755.397170] ret_from_fork+0x10/0x20
[ 2755.400745] task:jbd2/mmcblk1p2- state:R running task stack:0 pid:143 ppid:2 flags:0x00000008
[ 2755.410649] Call trace:
[ 2755.413087] __switch_to+0xe4/0x160
[ 2755.416573] __schedule+0x22c/0x660
[ 2755.420058] preempt_schedule_notrace+0x4c/0x70
[ 2755.424583] blk_mq_sched_insert_requests+0x104/0x250
[ 2755.429634] blk_mq_flush_plug_list+0xd8/0x240
[ 2755.434074] __blk_flush_plug+0xf0/0x140
[ 2755.437996] blk_finish_plug+0x38/0xf0
[ 2755.441742] jbd2_journal_commit_transaction+0xa2c/0x1710
[ 2755.447137] kjournald2+0xb8/0x254
[ 2755.450538] kthread+0x10c/0x110
[ 2755.453765] ret_from_fork+0x10/0x20
*****