Part Number: PROCESSOR-SDK-AM64X
Hi,
I am using latest TI SDK release www.ti.com/.../PROCESSOR-SDK-AM64X
PROCESSOR-SDK-LINUX-RT-AM64X — Processor SDK RT-Linux for AM64x Version: 09.00.00.03
For HSR I am following next doc to setup HSR with Linux HSR Offload Support
Also, I setup DTB overlay to configure eth1 and eth2 as PRU
By executing script from this link in chapter "Linux HSR Offload Support"
sh ./<script_filename.sh> hsr eth1 eth2 192.168.2.20
I see next messages:
remoteproc remoteproc13: unsupported resource 5
remoteproc remoteproc15: unsupported resource 5
QUESTION: what is this message and is it correct to have it?
Also, on same image I did next tests:
- disable all systemd services to start network interfaces on boot
- systemctl stop dhcpcd.service
- systemctl disable dhcpcd.service
- systemctl stop NetworkManager.service
- systemctl stop systemd-resolved.service
- systemctl disable NetworkManager.service
- systemctl disable systemd-resolved.service
- systemctl stop systemd-networkd
- systemctl disable systemd-networkd
- sync
- reboot the board and check if there is no any network up
root@am64xx-evm:~# ifconfig
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 96 bytes 7886 (7.7 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 96 bytes 7886 (7.7 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
root@am64xx-evm:~#
- execute hsr script
sh ./<script_filename.sh> hsr eth1 eth2 192.168.2.20
- I see next error
[ 55.732459] remoteproc remoteproc11: unsupported resource 5
[ 55.781782] icssg-prueth icssg1-eth eth1: timeout waiting for command done
[ 55.781806] icssg-prueth icssg1-eth eth1: TAS set state failed -110
[ 56.831683] remoteproc remoteproc14: unsupported resource 5
What are these errors and is there an impact on system?