Dear TI.
In MCU1_0, I can read gpio of GPIO0 group as below:
*(volatile unsigned int *)(0x00011C024) = 0x50007; //AJ20 GPIO0_9
*(volatile unsigned int *)(0x00011C04C) = 0x50007; //AJ21 GPIO0_18
GPIOSetDirMode_v0(CSL_GPIO0_BASE,9,GPIO_PIN_DIR_INPUT);
GPIOSetDirMode_v0(CSL_GPIO0_BASE,18,GPIO_PIN_DIR_INPUT);
tmp = GPIOPinRead_v0(CSL_GPIO0_BASE,9);
tmp = GPIOPinRead_v0(CSL_GPIO0_BASE,18);
But when I config and set GPIO1_4 of GPIO1 group :
*(volatile unsigned int *)(0x00011C214) = 0x10007; //V4 GPIO1_4
GPIOSetDirMode_v0(CSL_GPIO1_BASE,4,GPIO_PIN_DIR_OUTPUT);
GPIOPinWrite_v0(CSL_GPIO1_BASE,4,GPIO_PIN_VAL_LOW); //or write GPIO_PIN_VAL_HIGH (1)
And measure the voltage of V4. The voltage has not changed.
Please help check, and how to control GPIO1 group(GPIO1_4).
Thanks