This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: MCU2_1 PDK build error.

Part Number: TDA4VM

Please help to resolve the error,build inwindows10

input:make -s all_apps BOARD=j721e_evm CORE=mcu2_1

error:

#
# Combining RPRC images to generate multicore image....
# BINDIR is E:/code/tda4vm/ti-processor-sdk-rtos-j721e-evm-08_06_01_03/pdk_jacinto_08_06_01_03/packages/ti/binary/MCSPI_Baremetal_Master_TestApp/bin/j721e_evm CORELIST is mcu2_0 mcu2_1
# MULTICORE_IMG_PARAMS are 10 E:/code/tda4vm/ti-processor-sdk-rtos-j721e-evm-08_06_01_03/pdk_jacinto_08_06_01_03/packages/ti/binary/MCSPI_Baremetal_Master_TestApp/bin/j721e_evm/MCSPI_Baremetal_Master_TestApp_mcu2_0_release.rprc 11 E:/code/tda4vm/ti-processor-sdk-rtos-j721e-evm-08_06_01_03/pdk_jacinto_08_06_01_03/packages/ti/binary/MCSPI_Baremetal_Slave_TestApp/bin/j721e_evm/MCSPI_Baremetal_Slave_TestApp_mcu2_1_release.rprc 8 E:/code/tda4vm/ti-processor-sdk-rtos-j721e-evm-08_06_01_03/pdk_jacinto_08_06_01_03/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_freertos_mcu1_0_release.rprc
Number of Input Files 3
Error opening/creating out image file!
gmake[3]: *** [E:/code/tda4vm/ti-processor-sdk-rtos-j721e-evm-08_06_01_03/pdk_jacinto_08_06_01_03/packages/ti/drv/spi/example/mcspi_slavemode/mcspi_multicore_testapp.mk:69: force_multi_core_img_gen.c] Error -1
gmake[2]: *** [E:/code/tda4vm/ti-processor-sdk-rtos-j721e-evm-08_06_01_03/pdk_jacinto_08_06_01_03/packages/ti/build/makefile:367: MCSPI_Baremetal_MasterSlave_TestApp] Error 2
gmake[1]: *** [E:/code/tda4vm/ti-processor-sdk-rtos-j721e-evm-08_06_01_03/pdk_jacinto_08_06_01_03/packages/ti/build/makefile:128: MCSPI_Baremetal_MasterSlave_TestApp_has_dep] Error 2
make: *** [makefile:149: all_apps] Error 2