This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: VDDA_1P8_OLDI0 when OLDI0 is unused

Part Number: AM623

The AM623 clearly notes in table 6-74 connectivity requirements that the OLDI0 pins should be left unconnected when unused, but it doesn't offer any guidance for VDDA_1P8_OLDI0.

Can VDDA_1P8_OLDI0 be left unconnected  when unused?

At a minimum can the requirement for filtering the power supply be removed so that the pin can be tied directly to an existing supply?

Regards,

John

  • Hello John, 

    Thank you for the query.

    Can VDDA_1P8_OLDI0 be left unconnected  when unused?

    It is recommended to connect the recommended supplies as per the data sheet.

    At a minimum can the requirement for filtering the power supply be removed so that the pin can be tied directly to an existing supply?

    Don't see this as a concern. It is recommended to place a 0.1 uF decap near to the OLDI supply pin.

    Regards,

    Sreenivasa