Is there an example project that demonstrates how to convert a raw RGB image captured from a senosr to a YUV 4:2:2 image using the VPFE IPIPE. My target platform is the DM643X
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
abtreelph,
Are you using any of the BIOS PSP?
Regards,
Sandeep k
Hi abtreelph,
Apologies for the delayed response.
Please refer the section 4.1/4.2 of the "psp_1_00_02_00\pspdrivers\drivers\previewer\docs\BIOS_PREVIEWER_Driver_UserGuide.pdf" which has the explanation on the application which takes the raw image in bayer pattern and then converts it into the YVU 4:2:2 image.
Thanks and Regards,
Sandeep K