Hi,
I am trying to load IPC example for MCU2_0 core using the Linux running from A72 core. I have customized the memory map for IPC example, increased the DDR size for the MCU2_0 core and tried to load using the linux. I have made all the necessary changes in the k3-j721e-rtos-memory-map.dtsi File, I have increased the CORE memory region size, but still getting the errors , please help me resolve it.
I am getting the following errors
platform 5c00000.r5f: configured R5F for remoteproc mode
remoteproc remoteproc4: 5c00000.r5f is available
remoteproc remoteproc4: Booting fw image j7-main-r5f0_0-fw, size 530072
remoteproc remoteproc4: bad phdr da 0xa2000000 mem 0x84c00
remoteproc remoteproc4: Failed to load program segments: -22
Regards,
Surya