This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6412 SR2.0: when set the speed of ethernet to 10Mbps,the clock is still 25MHz,not 2.5MHz.

H i Sir,

   When we set the speed of ethernet to 10Mbps,the clock is still 25MHz,not 2.5MHz.

   We use SDK 08.06.00.42.

   I read the register address,"0x8000030" or "0x8000034", it always shows "0x00000003".

   But the clock is correct when the speed is 100M/1G bps.

   Could you provide any suggestion to me?

   Tnanks.

Best regards

Talmud