Part Number: TMS320C6747
Sir/madam,
I am using Codec AIC3106 and ADC6140 interfaced DSP TMS320C6747 via McAsp1 and McAsp0 ports.
Codec or ADC samples are read/written using EDMA peripheral. EDMA will generate interrupt after collecting/sending one frame of data i.e. 32 samples @16k Sampling rate i.e. frame duration is 2 msec.
I am using PING PONG buffer concept, hence I expect total absolute delay of 4 msec between audio input to audio output.
0th instant--> PING buffer is filled
2msec-->PING buffer processed and PONG buffer filled
4msec-->PING buffer filled and PONG buffer processed.
But, when I measured, I am getting absolute delay of 6.5 msec. This additional 2.5 msec delay is not understood. Please explain?
Measurement method.
Input: AM modulation with 50 Hz modulating input and 1 kHz carrier input and 90% modulation depth.
Difference between input peak to output peak is measured.
Snapshot of measurement is attached