This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tms320vc5416

Other Parts Discussed in Thread: TMS320VC5416

Hi,

will you please send me how to work the echo program given by texas.it will be very helpful for me.

 

                       with regards,

                          sharmi

  • Hi,

    Can you explain more detail?

    1. Where did you get the echo program?

    2. What hardware platform are you using?

    3. More detail what portion do you need a help?

    Regards,

    Hyun

  • Hi,

    1)I got the echo program given in CD by Texas(ti/tutorial/sim54x/echo.pjt) .

            2)I am using dsptms320vc5416 hardware from texas and i am using ccs v3.1.

    3)I am using echo program,when i am loading the program i come across with the following error.

    Error:File Loader error

    data verification failed at address 0xff80.please verify target memory and memory map,like this error is coming and again warning is coming

    Warning:

    RTDX configuration control

    RTDX target application does not match emulation protocol,loaded program was created with an RTDX library which does not match the target device.

    so the error occurs when i am loading tutorial programs only.please reply me as soon as earlier,it will be very useful for me

  • Hi,

    I solve the error which i faced.

    Thank you for your attention.I am having another doubt.Now I can load the program into the dsk kit.Can i work the echo program in realtime using MIC,SPEAKER.

    or only simulation can be done with this program,if I cant able to run this in realtime what i have to do.please send me reply as soon as earlier. 

     the program is in ti/tutorial/sim54x/echo for the dsp Tms320vc5416 hardware.

     

    Regards,

    Sharmi.

  • Hi,

     

    I referred the specified post.i want to work the echo program in realtime,in that post they have mentioned that codec to be added to the program to work in realtime.

    I am new one to this dsp5416,Will you please send me the program or guide me in doing this project.Thanks for your reply.

     

    Regards.

    Sharmi.