Hi,
I just upgraded the h264enc on the dm6446 platform to H264ENC.version.02.02.00.02.wizardversion.0.5.2. With everything else staying the same, the output fps at run-time is around 21. After just replacing the old h264enc (version H264ENC.version.02.02.00.02.wizardversion.0.5.2) back and rebuilding the codec-server, the output fps went back to 30.
I am targetting NTSC here.
So, believing the latest be the greatest, I think the latest h246enc should be better than the older ones. And also, I think I am seeing this fps issue because I am not setting the new algo right with old settings that work for the older version. But what are different? Sample application that comes with both releases is identical from source code. User's manual does not give any clue. So please help!
Thanks