I am using PCIe Interface of AM5706 (Gen 2.0). AM5706 will be root-complex and it will be configured as x1 lane of 2 ports. Whether this mode is compatible?
From Datasheet , I came to know it won't support both ports at Gen2.0, one will be as Gen1.0 (RC) and other port will be configured as Gen2.0(RC). Is it correct?
Two PCIe (PCIe_SS1 and PCIe_SS2) operates Gen2 1-lane supporting either RC or EP with the possibility of one operating in Gen1 and one in Gen2 - From Datasheet