Hi everyone,
I changed and combined few examples to one working in debug mode but attempt to run this using UART Boot Host failed. Another example ( also usage of McASP ) working in Debug mode works fine with UART2 using AIS Image. First thought was to tailor cmd file. Using the same cmd file from working example doesn;t help. Is it possible something else then cmd file is causing the trouble or should I try working on cmd files some more?