This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: Treating LBCLKO (N21) pin

Part Number: AM6442


Hi,

My customer needs to know as soon as possible about treating LBCLKO of OSPI on AM6442, because they have to fix their board design soon.

They’ve read the chapter 4.4.1 OSPI, xSPI, QSPI, SPI Boot in the TRM about the treating LBCLKO (Pin N21) when OSPI is used in Primary Boot Mode with the highest speed (using DQS), and there is the following description. However, the pin N21 is used as GPIO instead of LBCLKO on their prototype board.

In their use case also, do they have to follow the following when using OSPI at the highest speed in Primary Boot Mode ? The pin N21 itself must strictly adhere to the following ?

Or in the only case of pin N21 is selected as LBCLKO, the following should be required ?

If the use of the pin N21 itself is prohibited, they want to remove the resistor and leave it open. Will it be prohibited even leaving the wiring pattern as well? 

Regards,

Hideaki