Part Number: TDA4VM
Hello, please advise, how can I collect more detailed logs during a custom onnx model TIDL-accelerated inference on the development board?
Specifically, I have encountered 2 issues, where model inference works fine in the x86 docker container simulator (dockerfile is bundled with TIDL), but fails on the devboard:
1. inference fails with the following error message:
91692.403482 s: VX_ZONE_INIT:[tivxHostInitLocal:93] Initialization Done for HOST !!!
91692.444839 s: VX_ZONE_ERROR:[ownContextSendCmd:802] Command ack message returned failure cmd_status: -1
91692.444869 s: VX_ZONE_ERROR:[ownContextSendCmd:838] tivxEventWait() failed.
91692.444903 s: VX_ZONE_ERROR:[ownNodeKernelInit:525] Target kernel, TIVX_CMD_NODE_CREATE failed for node TIDLNode
91692.444923 s: VX_ZONE_ERROR:[ownNodeKernelInit:526] Please be sure the target callbacks have been registered for this core
91692.444941 s: VX_ZONE_ERROR:[ownNodeKernelInit:527] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
91692.444959 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 0, kernel com.ti.tidl:1:1 ... failed !!!
91692.444980 s: VX_ZONE_ERROR:[vxVerifyGraph:2055] Node kernel init failed
91692.444999 s: VX_ZONE_ERROR:[vxVerifyGraph:2109] Graph verify failed
TIDL_RT_OVX: ERROR: Verifying TIDL graph ... Failed !!!
TIDL_RT_OVX: ERROR: Verify OpenVX graph failed
2. devboard hangs indefinitely with the following messages in log:
libtidl_onnxrt_EP loaded 0xd6b3350
Final number of subgraphs created are : 1, - Offloaded Nodes - 404, Total Nodes - 404
APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=4) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
953960.137830 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
953960.141201 s: VX_ZONE_INIT:Enabled
953960.141213 s: VX_ZONE_ERROR:Enabled
953960.141221 s: VX_ZONE_WARNING:Enabled
953960.141965 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
953960.142953 s: VX_ZONE_INIT:[tivxHostInitLocal:93] Initialization Done for HOST !!!
(hangs)
Could you please advise on how I can extract more logs in order to understand and troubleshoot such errors?
(the above was tried with tidl_tools tags 08_06_00_02 and 08_06_00_03 on SDK versions 08_06_00_38 and 08_06_00_11 accordingly,
and changing `debug_level` compilation option in TIDL does not make a difference)
)
Regards,
Aleksandr