This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[C6727] burning flash for bootloader

hi

I'm working with c6727 (CCS 3.3)and I configured my dsp to boot from parallel flash. 

I worte secondary bootloader and then I tried  to burn it into the flash(at its begining address as requierd).

I use the same files hex6.exe to convert my .out file to .dat file(burning file) as i used at c6713(CCS 3.1).

the result is file filled with alot of 0.

Is a different conversion requiered for .out files created for 6727 ?

where can I get those files?(if existing)

thanks

mano