This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROBLEM ABOUT THE C6720 BOOTLOADER



Refer To THE application note document SPRAA69C,THE C6720DSP CAN  USE the HCS,SPI0SOMI,SPI0SIMO AND SPICLK pins to select boot mode , but the RFP package does not provide the HCS pin,,,the question is,how to do the bootload mode selection.or i dont  have to care about the HCS pin when using the RFP ,or  additional pins will be used ?

  • Hello Tim,

    As you have already noted the C6720 RFP package does not contain the UHPI peripheral, and therefore you will not have access to the UHPI_HCS pin. For this device and package the UHPI_HCS can be considered internally pulled high. This will still allow you to configure the device to boot from the other 5 boot modes.