Hi,
When I running the following commands:
$ sudo ../../../../build/tools/mktarball.sh ../../../host/linux-x86/bin/fs_get_stats android_rootfs . rootfs rootfs.tar.bz2
The feedback is
../../../../build/tools/mktarball.sh: line 20: cd: android_rootfs: No such file or directory
And then it start to build,
At the beginning 1.0G is very fast, but after this it is running very very slow.
I start in yesterday 3:00pm, it is still running but the size of file is 1.33G.
I leave it to run over night.
Is it this correct?What make it too slow?
I follow all in TI Android GingerBread 2.3 DevKit 1.0 Developers Guide to build.