This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP

Hi

In our application we need to capture voice data (100Hz-3.3khz) , data from a single microphone (mono).

Audio sample rate is 8kS/s We need to compress this data using ACELP , CELP. Also there should be a feature for VAD(Voice activity detection).

Other interfaces we require are 2 I2C interface.

Interface for external RAM for a minimum size of 256kByte.

An SD card interface. Our system is a battery powered one . Please suggest some processor (DSP/microcontroller) for this application.

If built in libraries are available for ACELP, CELP compression technique and for VAD then this will speed up our implementation.