Part Number: AM3354
Hi,
My customer has developed HMI product with AM3354. In this product, the screen display is disturbed occasionally when the SD card is accessed.
As they have some questions, could you answer their questions below ?
1) As the first phenomenon of LCD display disturbance, LCD Data becomes Low for a certain period of time.
They presume that this is the result of DMA (Direct Memory Access) conflict between the timing of reading/writing the SD card and the drawing processing of the LCD.
Is their understanding correct?
2) They also found similar LCD display disturbances in TI's FAQ. AM3359 Timing - Processors forum - Processors - TI E2E support forums
Is it correct to think that this issue can also be resolved by adjusting the OCP_CONFIG register setting value?
3) The LCD Data becomes Low (= black screen display) for one LCD drawing cycle in the next drawing cycle when the LCD Data is delayed by several us compared with when it is normal.
Is this the specification of the AM3354?
< Problem >
Flicker occasionally occurs on the screen during reading/writing SD card.
There are two kinds of flicker phenomena.
1) The screen display shifts in the horizontal direction.
2) The screen becomes dark (Black screen display).
However, any phenomenon automatically returns to correct display.
< Occurrence Condition >
Read/Write SD card
< Occurrence Frequency >
This problem occurred maximum 25 times in 1 hour when reading/writing SD card are repeated in succession.
Please see the attached file for the details with some waveforms and pictures.
Thanks and regards,
Hideaki