I am working on OMAP-L137, in this SPI0 is muxed with SPI0_ENA/UART0_CTS/EQEP0A/GPIO5[3]/BOOT[3] similarly other
pins of SPI0 are also muxed with other pins of other peripheral module. We are using OMAP-L137 EVM board, in this BOOT[3]
is used to select Boot mode which can be configured through SW2 switch which determine the source for processor booting.
After booting is completed, can i change this switch setting i.e. BOOT[3] to SPI0_ENA so that i can read & write to SPI Flash?