Part Number: SK-TDA4VM
Hello Champs,
sdk: ti-processor-sdk-linux-j7-evm-08_06_01_02
Camera:imx219
Customer has referenced below document to configure the imx219:In /run/media/mmcblk0p1/uEnv.txt, modify name_overlays=k3-j721e-sk-rpi-cam-imx219.dtbo
Problem: using v4l2 API ,format:V4L2_PIX_FMT_SRGGB8,width:640,height:480, it prompted: stuck in DQBUF
root@tda4vm-sk:/home# gcc camera.c
root@tda4vm-sk:/home# ./a.out
Open /dev/video2 succeed - 3
Open /dev/v4l-subdev2 succeed
------- VIDIOC_QUERYCAP ----
driver: j721e-csi2rx
card: j721e-csi2rx
bus_info: platform:4500000.ticsi2rx
version: 5.10.162
capabilities: A5200001
Video Capture
Read / Write
Streaming
VIDIOC_S_FMT succeed!
width 640, height 480, size 307200, bytesperline 640, format RGGB
VIDIOC_REQBUFS succeed!
Memory map succeed!
VIDIOC_QBUF succeed!
VIDIOC_STREAMON succeed!
1. Is there something missed when configuring the imx210?
2. Does it need to configure the CSI?
3. How to resolve the DQBUF issue?
Thanks
Regards
Shine