This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BYTES-3P-BE-AM6254: OLDI LVDS and CSI signal integrity tuning and electrical specifications

Part Number: BYTES-3P-BE-AM6254

Hi,

We have used LVDS interface in our design.

Can we tune this signal with controlling LVDS interface control register? 

We found below relevant control register but no further detail found in TRM docs, Please suggest possible control option to finetune this clock levels.
2.1.1.284 CTRL_MMR0_OLDI0_CLK_IO_CTRL_PROXY Register (Offset = A610h) [reset = c1043008h ]

Share CSI acceptable limit specification for acceptable eye width and height and allowable jitter value.

  • Hello Kalpesh Diyora

    Thank you for the query.

    We have used LVDS interface in our design.

    Can we tune this signal with controlling LVDS interface control register? 

    We found below relevant control register but no further detail found in TRM docs, Please suggest possible control option to finetune this clock levels.
    2.1.1.284 CTRL_MMR0_OLDI0_CLK_IO_CTRL_PROXY Register (Offset = A610h) [reset = c1043008h ]

    Can you please share additional details on the use case including any issues you are facing.

    Share CSI acceptable limit specification for acceptable eye width and height and allowable jitter value.

    I assume the above query is for the OLDI and this is for the CSI.

    I need more details on your requirements. We recommend discussing a specific topic per thread to be able to assign to the experts as required. 

    Could you please start a new thread specific to the CSI related queries.

    Regards,

    Sreenivasa

  • Hello Kalpesh Diyora

    Please refer below input i received from the display expert

    600h 32 MAIN_CTRL_MMR_OLDI0_DAT0_IO_CTRL 0010 8600h
    8604h 32 MAIN_CTRL_MMR_OLDI0_DAT1_IO_CTRL 0010 8604h
    8608h 32 MAIN_CTRL_MMR_OLDI0_DAT2_IO_CTRL 0010 8608h
    860Ch 32 MAIN_CTRL_MMR_OLDI0_DAT3_IO_CTRL 0010 860Ch
    8610h 32 MAIN_CTRL_MMR_OLDI0_CLK_IO_CTRL 0010 8610h
    Do we allow customer to tweek these registers for OLDI

     Nope, we need their default values only.

     We only change oldi-pd-control

     What does the PD control do - does it power down when not used?

     By default it's powered down. We turn OLDI IOs on with that.

    Regards,

    Sreenivasa