This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This information applies to Linux SDK Version 9.0 and prior. For more up to date information, refer to this FAQ: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1494485/faq-processor-sdk-getting-started-with-gpios-in-linux-using-the-am62-and-am64-family-processors
I am familiar with SYSFS interface to interact with GPIO pins. In SDK 9.0, this interface for GPIO was removed. How can I use the Chardev interface? This is for the AM62x and AM64x.
In SDK 9.0, the legacy SYSFS interface for GPIO was removed and the Chardev interface takes its place. This FAQ will introduce the Chardev interface and how to get started.
Chardev Interface
The Character Device (Chardev) Interface uses the gpiod library to interact with GPIO pins in userspace. It uses commands in the EVM terminal to perform the same operations that SYSFS does.
Read about these commands in the Manpages: https://manpages.debian.org/experimental/gpiod/index.html
Here is a quick overview of the commands:
Commands |
Function |
gpiodetect |
This shows the different gpiochip available, addresses, and pin count. |
gpiofind |
This finds a gpiochip and line number based on the name of the pin. Most of the pins do not have a name. |
gpioget |
This returns the value of a pin. This command will change the direction of the pin to input. |
gpioinfo |
This shows information about gpiochips like direction and name. |
gpiomon |
This is a monitor to detect changes in value. |
gpioset |
This sets the value of a pin. This command will change the direction of the pin to output. |
SYSFS vs Chardev
Here are some of the benefits of using Chardev over SYSFS:
The only drawback of using Chardev over SYSFS is lack of control over pin direction. gpioset and gpioget are commands that will change the direction of the pin and requires cautious use of these commands. With Chardev, changing the direction of a pin will erase the current value of the pin and set it to undefined.
An example:
If a user sets a pin value using gpioset then tries to read the value using gpioget , the outcome is unexpected. The direction was changed due to these commands and the value will differ from hardware and software. From the software perspective, the value will be whatever the default value is (usually 1/high). From the hardware perspective, the measured voltage will be around .5V to .7V which means its undefined (High=3.3V and Low=0V).
Replicating SYSFS process with Chardev
For SYSFS, the steps to set a pin include:
The Chardev interface can complete steps 3 and 4 in the same command line. Steps 1 and 2 for SYSFS are removed since they are unneeded, but a different step will be used. Here is how this process can be replicated with Chardev:
Lets work through an example of GPIO0_39 using both interfaces to see the differences.
Example with GPIO0_39
Starting with SYSFS:
# cd /sys/class/gpio/ # ls -l #step 1 total 0 --w------- 1 root root 4096 Feb 24 04:51 export lrwxrwxrwx 1 root root 0 Feb 24 04:51 gpiochip287 -> ../../devices/platform/bus@f0000/20010000.i2c/i2c-1/1-0022/gpio/gpiochip287 lrwxrwxrwx 1 root root 0 Feb 24 04:51 gpiochip311 -> ../../devices/platform/bus@f0000/601000.gpio/gpio/gpiochip311 lrwxrwxrwx 1 root root 0 Feb 24 04:51 gpiochip399 -> ../../devices/platform/bus@f0000/600000.gpio/gpio/gpiochip399 lrwxrwxrwx 1 root root 0 Feb 24 04:51 gpiochip486 -> ../../devices/platform/bus@f0000/bus@f0000:bus@4000000/4201000.gpio/gpio/gpiochip486 lrwxrwxrwx 1 root root 0 Feb 24 04:51 gpiochip510 -> ../../devices/platform/bus@f0000/3b000000.memory-controller/gpio/gpiochip510 --w------- 1 root root 4096 Feb 24 04:51 unexport # echo 438 > export #step 2 # cd gpio438 # echo out > direction #step 3 # echo 1 > value #step 4
To get gpio438, we matched the base address of GPIO0 (0x600000) to the gpiochip base number(gpiochip399). This means the base number for GPIO0 is 399. Then we add the offset number of the pin (39) to the base to get 438. Finally, it was exported.
Please note GPIO1 has an address of 0x601000 and MCU_GPIO0 has an address of 0x4201000.
Using the SYSFS interface, GPIO0_39 is an output with value 1. Let's get the same result with Chardev interface:
Chardev:Fullscreen1234567891011# gpiodetect #step 1gpiochip0 [4201000.gpio] (24 lines)gpiochip1 [600000.gpio] (92 lines)gpiochip2 [601000.gpio] (52 lines)gpiochip3 [1-0022] (24 lines)# gpioset gpiochip1 39=1 #step 2XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX# gpiodetect #step 1 gpiochip0 [4201000.gpio] (24 lines) gpiochip1 [600000.gpio] (92 lines) gpiochip2 [601000.gpio] (52 lines) gpiochip3 [1-0022] (24 lines) # gpioset gpiochip1 39=1 #step 2
Since GPIO0 has a base address of 0x600000, gpiodetect tells us that gpiochip1 corresponds to GPIO0.
Please note GPIO1 has an address of 0x601000 and MCU_GPIO0 has an address of 0x4201000.
GPIO0_39 is an output with value 1 just like SYSFS interface. Notice the following:
From here, explore some of the other commands available in the Chardev interface like gpiomon for event polling and gpioinfo for more information about pins.