Part Number: TDA4VM
HI expert
-system : PDK 7.1 + QNX + OSPI boot + SBL
We are using the HS-SE board it is signed our company custom key
An issue not found in HS-SE TIDK arises from HS-SE. Authentication fails when loading ATF from can_boot_app.
This error occurs ones during 20-30 power on and off tests.
below mcu uart log
TIFS ver: 20.8.7--v2020.08d (Terrific Lla
Verify Failed For the Img at offset 0x200000 CertLoadAddr 0xba800000!!
Boot Halted!!
Repeated calls to the Scicclient_procBootAuthAndStart of the SBL_VerifyMulticoreImage(file:sbl_soc.c) function resolve the issue.
Please check if this is the right solution.