This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Project compile error



This may be very simple, but I cannot get it to work. Here is the story, I've added the line #include <linux/interrupt.h> and I get the following error:

/home/jhernandez/EUCDK/eucdk_ov_15/ti-davinci/include/linux/interrupt.h:11, from avServerMain.c:23:

/home/jhernandez/EUCDK/eucdk_ov_15/ti-davinci/include/linux/hardirq.h:62:3: error: #error PREEMPT_ACTIVE is too low!

make[7]: *** [depend] Error 1

make[7]: Leaving directory `/home/jhernandez/EUCDK/eucdk_ov_15/av_capture/application/ipnc/multimedia/av_server/src/common'

make[6]: *** [libs] Error 2

make[6]: Leaving directory `/home/jhernandez/EUCDK/eucdk_ov_15/av_capture/application/ipnc/multimedia/av_server'

make[5]: *** [depend] Error 2

make[5]: Leaving directory `/home/jhernandez/EUCDK/eucdk_ov_15/av_capture/application/ipnc/multimedia/av_server'

make[4]: *** [libs] Error 2

make[4]: Leaving directory `/home/jhernandez/EUCDK/eucdk_ov_15/av_capture/application/ipnc'

make[3]: *** [depend] Error 2

make[3]: Leaving directory `/home/jhernandez/EUCDK/eucdk_ov_15/av_capture/application/ipnc'

make[2]: *** [libs] Error 2

make[2]: Leaving directory `/home/jhernandez/EUCDK/eucdk_ov_15'

make[1]: *** [depend] Error 2

make[1]: Leaving directory `/home/jhernandez/EUCDK/eucdk_ov_15'

make: *** [exe] Error 2

 

 Why I can't do this? I should be albe to do it....