This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: failed to request resources for 46000000.ethernet-tx7 (irq 103) on irqchip MSI-INTA

Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH

Hi experts,

        I am currently using the TDA4VH development board with SDK 8.6.

 I am using the cpsw9g switch in native driver mode and I want to send packets through eth0 of the cpsw2g switch. Therefore, I have made the following configuration.

ifconfig eth0 down

ifconfig eth0 hw ether 00:11:22:33:44:01

ethtool -L eth0 tx 8

ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off

ifconfig eth0 up

sleep 6

# add vlan

vconfig add eth0 11


sleep 2

# set qbv
base=0

tc qdisc replace dev eth0 parent root handle 100 taprio \
    num_tc 8 \
    map 0 1 2 3 4 5 6 7 0 0 0 0 0 0 0 0 \
    queues 1@0 1@1 1@2 1@3 1@4 1@5 1@6 1@7 \
    base-time ${base} \
    sched-entry S 40 200000 \
    sched-entry S bf 4800000 \
    flags 2

ip link set eth0.11 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
ifconfig eth0.11 192.168.11.1
echo "eth0 set ok!"

But when I run it, I get the following error:

root@j784s4-evm:~/tsn_test_tda4_1/qbv_test# ./set_eth0.sh
[  111.333088] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
[  111.351108] genirq: Failed to request resources for 46000000.ethernet-tx7 (irq 103) on irqchip MSI-INTA
[  111.360502] am65-cpsw-nuss 46000000.ethernet: failure requesting tx7 irq 103, -22
[  111.368028] am65-cpsw-nuss 46000000.ethernet: Failed to add tx NAPI -22
netlink error: Invalid argument
[  111.390965] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[  111.400464] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  113.071150] br0: port 1(eth1) entered disabled state
[  113.076118] am65-cpsw-nuss c000000.ethernet eth1: Link is Down
[  115.119496] am65-cpsw-nuss c000000.ethernet eth1: Link is Up - 1Gbps/Full - flow control rx/tx
[  115.128150] br0: port 1(eth1) entered blocking state
[  115.133110] br0: port 1(eth1) entered forwarding state
[  115.503489] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[  115.512205] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[  117.424216] 8021q: 802.1Q VLAN Support v1.8
[  117.428429] 8021q: adding VLAN 0 to HW filter on device eth0
[  117.434128] 8021q: adding VLAN 0 to HW filter on device eth1
[  117.439797] 8021q: adding VLAN 0 to HW filter on device eth2
[  117.445462] 8021q: adding VLAN 0 to HW filter on device eth3
[  117.451126] 8021q: adding VLAN 0 to HW filter on device eth4
[  117.456791] 8021q: adding VLAN 0 to HW filter on device eth5
[  117.462877] am65-cpsw-nuss 46000000.ethernet: Adding vlan 11 to vlan filter
[  117.469929] am65-cpsw-nuss 46000000.ethernet: get: wrong ale fld id 2
[  117.476362] am65-cpsw-nuss 46000000.ethernet: get: wrong ale fld id 1
eth0 set ok!
root@j784s4-evm:~/tsn_test_tda4_1/qbv_test# [  129.582007] ------------[ cut here ]------------
[  129.586625] NETDEV WATCHDOG: eth0 (am65-cpsw-nuss): transmit queue 7 timed out
[  129.593869] WARNING: CPU: 0 PID: 0 at net/sched/sch_generic.c:467 dev_watchdog+0x320/0x328
[  129.602110] Modules linked in: 8021q garp mrp sch_taprio bridge stp llc bluetooth ecdh_generic ecc rfkill cdns3 udc_core roles usbcore cdns_csi2rx rpmsg_c6
[  129.656811] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G           O      5.10.162-g76b3e88d56 #1
[  129.665312] Hardware name: Texas Instruments J784S4 EVM (DT)
[  129.670954] pstate: 20000005 (nzCv daif -PAN -UAO -TCO BTYPE=--)
[  129.676942] pc : dev_watchdog+0x320/0x328
[  129.680936] lr : dev_watchdog+0x320/0x328
[  129.684928] sp : ffff8000112bbdb0
[  129.688229] x29: ffff8000112bbdb0 x28: ffff0008022cf940
[  129.693526] x27: 0000000000000004 x26: 0000000000000140
[  129.698822] x25: 00000000ffffffff x24: 0000000000000000
[  129.704118] x23: ffff0008022ce3dc x22: ffff0008022ce000
[  129.709414] x21: ffff0008022ce480 x20: ffff800011117000
[  129.714710] x19: 0000000000000007 x18: 0000000000000010
[  129.720006] x17: 0000000000000000 x16: 0000000000000000
[  129.725302] x15: ffff800011121f10 x14: 00000000000002a7
[  129.730598] x13: ffff800011121f10 x12: 00000000ffffffea
[  129.735894] x11: ffff8000111a05b0 x10: ffff800011188570
[  129.741190] x9 : ffff8000111885c8 x8 : 0000000000017fe8
[  129.746486] x7 : c0000000ffffefff x6 : 0000000000000003
[  129.751782] x5 : 0000000000000000 x4 : 0000000000000000
[  129.757078] x3 : 0000000000000100 x2 : 0000000000000100
[  129.762374] x1 : 0f219d646ae3c500 x0 : 0000000000000000
[  129.767670] Call trace:
[  129.770105]  dev_watchdog+0x320/0x328
[  129.773757]  call_timer_fn.isra.0+0x24/0x80
[  129.777925]  run_timer_softirq+0x400/0x438
[  129.782007]  efi_header_end+0x120/0x268
[  129.785829]  irq_exit+0xc0/0xe0
[  129.788957]  __handle_domain_irq+0x68/0xc0
[  129.793040]  gic_handle_irq+0x58/0x128
[  129.796774]  el1_irq+0xcc/0x180
[  129.799904]  arch_cpu_idle+0x18/0x28
[  129.803466]  default_idle_call+0x20/0x68
[  129.807375]  do_idle+0xc0/0x128
[  129.810502]  cpu_startup_entry+0x24/0x60
[  129.814410]  rest_init+0xd4/0xe4
[  129.817627]  arch_call_rest_init+0x10/0x1c
[  129.821707]  start_kernel+0x478/0x4b0
[  129.825355] ---[ end trace 93eb64b1304599a2 ]---
[  129.829971] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:10320 dql_avail:-134 free_desc:515
[  131.342229] Initializing XFRM netlink socket
[  135.470018] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:15964 dql_avail:-134 free_desc:515
[  140.590006] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:21084 dql_avail:-134 free_desc:515
[  145.454006] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:25948 dql_avail:-134 free_desc:515
[  150.574013] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:31068 dql_avail:-134 free_desc:515
[  155.438004] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:35932 dql_avail:-134 free_desc:515
[  160.558003] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:41052 dql_avail:-134 free_desc:515
[  165.422007] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:45916 dql_avail:-134 free_desc:515
[  170.542005] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:51036 dql_avail:-134 free_desc:515
[  175.662005] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:56156 dql_avail:-134 free_desc:515
[  181.550007] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:62044 dql_avail:-134 free_desc:515
[  186.414006] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:66908 dql_avail:-134 free_desc:515
[  191.534006] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:72028 dql_avail:-134 free_desc:515
[  196.654005] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:77148 dql_avail:-134 free_desc:515
[  202.542007] am65-cpsw-nuss 46000000.ethernet eth0: txq:7 DRV_XOFF:0 tmo:83036 dql_avail:-134 free_desc:515

I have set up the same environment on another TDA4VH board and executed the same command. Strangely, it runs perfectly fine on that board. What could be the reason for this discrepancy?

The correct execution screenshot is shown below.

regards

yrq