A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DSP C5504 is connected to external Codec via SPI (control data) and via I2S0 – sound data. Codec is configured as master in I2S interface and DSP – as slave. Word format is 32 bits. DSP receives all sound data from Codec, but does not transmit to codec anything. We watch by scope pin I2S0_CLK=750kHz, pin I2S0_FS=11.72 KHz, but DSP output I2S0_DX is low constantly. When DSP has configured as master, Sound Data is transmitted via I2S0_DX to Codec. Why Sound data is not transmitted from DSP when it is in slave mode? Thanks Sergey Zevelev