This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA829V: PCIe RC mode registers restriction

Part Number: DRA829V

Hi team,

Currently, in my customer's system the following registers are restricted in PCIe RC mode.

・NUM_bits(*1) of PCIe_core_ATU_wrapper_OB_I_addr0 Register 

・Region_size(*1) of the PCIe_core_ATU_wrapper_OB_I_AXI_addr0 Register 

(*1) Refer to J721E_registers4.PDF

When they checked the operation of the above field setting, it was only effective up to 16MB (NUM_bits = region_size = 0x18).

1. Is it possible to operate with a specified size of 16MB or more?

2. If the above (1) is possible, please tell us which register to check or set. 

Thank you in advance.

Best Regards,

Kenley