This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5514 Bootloader SARAM usage



The C5514 Booloader document   http://focus.ti.com/lit/an/sprabd7/sprabd7.pdf section 1.2 states that SARAM31 is reserved for the bootloader. SARAM31 does not exist on the C5514 chip according to the C5514 datasheet. The SARAM31 location on the C5514 is listed as Reserved

For the C5514 does the bootloader use some "reserved" memory space located at the C5515 SARAM31 byte address 0x4E000-0x4FFFF?

-or-

Does the bootloader use SARAM23 since it is the last available SARAM location on the chip?

 

Any idea if this applies to the C5504 chip as well?