U-Boot 2010.06 (Mar 14 2011 - 20:52:37)
DRAM: 2 GiB
Using default environment
The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is alr
eady flashed
Hit any key to stop autoboot: 3 2 1 0
mmc1 is available
reading u-boot.bin
177860 bytes read
## Starting application at 0x80800000 ...
U-Boot 2010.06 (Mar 14 2011 - 18:18:40)
I2C: ready
DRAM: 2 GiB
NAND: HW ECC Hamming Code selected
256 MiB
.:;rrr;;.
,5#@@@@#####@@@@@@#2,
,A@@@hi;;;r5;;;;r;rrSG@@@A,
r@@#i;:;s222hG;rrsrrrrrr;ri#@@r
:@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@:
B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B
@@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@
@@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@
@@;;rrsrrs@MB#@@@@@###@@@@@@#rsrsrsrsrr;;@@
G@r;rrsrsr;#X;SX25Ss#@@#M@#9H9rrsrsrsrsrs;r@G
@9:srsrsrs;2@;:;;:.X@@@@@H::;rrsrsrsrsrsrr:3@
X@;rrsrsrsrr;XAi;;:&@@#@Bs:rrsrsrsrsrsrsrsrr;@X
@#;rsrsrsrsrr;r2ir@@@###::rrsrsrsrsrsrsrsrsr:@@
@A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@
@&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@
@#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@
M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@#
:@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@,
@@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@
@A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@
;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@;
r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r
,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@,
B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H
.@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@.
.A@@#5r;;;r;;;rrr;r:r#AsM@@H.
;&@@@@MhXS5i5SX9B@@@@G;
:ihM#@@@@@##hs,
Net: Detected MACID:80:0:0:0:0:50
cpsw
Hit any key to stop autoboot: 3 0
TI8148_EVM#
TI8148_EVM#
TI8148_EVM#mmc init
mmc1 is available
TI8148_EVM#setenv bootargs 'console=ttyO0,115200n8 root=/dev/mmcblk0p2 rootdelay
=2 rootfstype=ext3 mem=128M'
TI8148_EVM#fatload mmc 1 0x81000000 uImage
reading uImage
2248264 bytes read
TI8148_EVM#bootm 0x81000000
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37-rc3
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2248200 Bytes = 2.1 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37-rc3 (root@pcz-mmalab55) (gcc version 4.3.3 (Sourcery G++ Li
te 2009q1-203) ) #2 Wed Aug 3 16:28:06 IST 2011
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148evm
reserved size = 0 at 0
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512
Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rootdelay=2 root
fstype=ext3 mem=128M
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 128MB = 128MB total
Memory: 125108k/125108k available, 5964k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xc8800000 - 0xf8000000 ( 760 MB)
lowmem : 0xc0000000 - 0xc8000000 ( 128 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0033000 ( 172 kB)
.text : 0xc0033000 - 0xc0441000 (4152 kB)
.data : 0xc0442000 - 0xc047a260 ( 225 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:368
GPMC revision 6.0
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 599.65 BogoMIPS (lpj=2998272)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
registered ti814x_vpss device
pm_dbg_init: only OMAP3 supported
Registered ti81xx_fb device
Could not look up wd_timer-1 hwmod
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c_omap i2c_omap.1: bus 1 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
Switched to NOHz mode on CPU #0
musb_hdrc: version 6.0, cppi4.1-dma, host, debug=0
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
musb_hdrc musb_hdrc.0: MUSB HDRC host driver
musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb_hdrc musb_hdrc.0: USB Host mode controller at c880c000 using DMA, IRQ 18
musb_hdrc musb_hdrc.1: MUSB HDRC host driver
musb_hdrc musb_hdrc.1: new USB bus registered, assigned bus number 2
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb_hdrc musb_hdrc.1: USB Host mode controller at c881e800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 244
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap-hsuart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled
omap-hsuart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap-hsuart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap-hsuart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap-hsuart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap-hsuart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
ahci ahci: forcing port_map 0x0 -> 0x1
ahci ahci: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc apst
scsi0 : ahci
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
omap2-nand driver initializing
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
Creating 6 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffd
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
i2c /dev entries driver
PSTATE 1ff0000
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
1-0018 supply IOVDD not found, using dummy regulator
1-0018 supply DVDD not found, using dummy regulator
1-0018 supply AVDD not found, using dummy regulator
1-0018 supply DRVDD not found, using dummy regulator
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
#0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
Detected MACID=0:0:0:0:0:0
Waiting 2sec before mounting root device...
ata1: SATA link down (SStatus 0 SControl 300)
mmc0: new high speed SD card at address 0007
mmcblk0: mmc0:0007 SU02G 1.83 GiB
mmcblk0: p1 p2
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing init memory: 172K
mmcblk0: retrying using single block read
mmcblk0: error -110 sending read/write command, response 0x0, card status 0x800b
00
mmcblk0: error -110 transferring data, sector 2372817, nr 8, card status 0x800b0
0
end_request: I/O error, dev mmcblk0, sector 2372817
mmcblk0: error -110 sending read/write command, response 0x0, card status 0x400b
00
mmcblk0: error -110 transferring data, sector 2372818, nr 7, card status 0x400b0
0
end_request: I/O error, dev mmcblk0, sector 2372818
mmcblk0: error -110 sending read/write command, response 0x0, card status 0x400b
00
mmcblk0: error -110 transferring data, sector 2372819, nr 6, card status 0x400b0
0
end_request: I/O error, dev mmcblk0, sector 2372819
mmcblk0: error -110 sending read/write command, response 0x0, card status 0x400b
00
mmcblk0: error -110 transferring data, sector 2372820, nr 5, card status 0x400b0
0
end_request: I/O error, dev mmcblk0, sector 2372820
mmcblk0: error -110 sending read/write command, response 0x0, card status 0x400b
00
mmcblk0: error -110 transferring data, sector 2372821, nr 4, card status 0x400b0
0
end_request: I/O error, dev mmcblk0, sector 2372821
mmcblk0: error -110 sending read/write command, response 0x0, card status 0x400b
00
mmcblk0: error -110 transferring data, sector 2372822, nr 3, card status 0x400b0
0
end_request: I/O error, dev mmcblk0, sector 2372822
mmcblk0: error -110 sending read/write command, response 0x0, card status 0x400b
00
mmcblk0: error -110 transferring data, sector 2372823, nr 2, card status 0x400b0
0
end_request: I/O error, dev mmcblk0, sector 2372823
mmcblk0: error -110 sending read/write command, response 0x0, card status 0x400b
00
mmcblk0: error -110 transferring data, sector 2372824, nr 1, card status 0x400b0
0
end_request: I/O error, dev mmcblk0, sector 2372824
EXT3-fs error (device mmcblk0p2): ext3_find_entry: reading directory #61698 offs
et 0
mmcblk0: error -110 sending read/write command, response 0x0, card status 0x400b
00
mmcblk0: error -110 transferring data, sector 144585, nr 8, card status 0x0
I am booting ti j4 board.
I am using the prebuilt binaries came with ezsdk package.
Boot args as:
mmc init
setenv bootargs 'console=ttyO0,115200n8 root=/dev/mmcblk0p2 rootdelay=2 rootfstype=ext3 mem=128M'
fatload mmc 1 0x81000000 uImage
bootm 0x81000000
But,
am getting the bellow error
mmcblk0: error -110 sending read/write command, response 0x0, card status 0x800b00
mmcblk0: error -110 transferring data, sector 2372817, nr 8, card status 0x800b00
end_request: I/O error, dev mmcblk0, sector 2372817