This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VL-Q1: Error while installing TI SDK RTOS 09.00.00.02 for j721s2

Part Number: TDA4VL-Q1

While making flatbuffers 1.12.0 dependent software, I'm getting the following error.

(TISDK_9_0) che7@che7-server2:~/Desktop/sourav/flatbuffers-1.12.0$ make
Consolidate compiler generated dependencies of target flatbuffers
[  5%] Built target flatbuffers
Consolidate compiler generated dependencies of target flatc
[ 40%] Built target flatc
Consolidate compiler generated dependencies of target flathash
[ 42%] Built target flathash
[ 43%] All generated files were updated.
[ 57%] Built target generated_code
Consolidate compiler generated dependencies of target flattests
[ 58%] Building CXX object CMakeFiles/flattests.dir/tests/test.cpp.o
In file included from /home/che7/Desktop/sourav/flatbuffers-1.12.0/tests/test.cpp:39:
/home/che7/Desktop/sourav/flatbuffers-1.12.0/tests/arrays_test_generated.h: In constructor ‘MyGame::Example::ArrayStruct::ArrayStruct(float, int8_t, int32_t)’:
/home/che7/Desktop/sourav/flatbuffers-1.12.0/tests/arrays_test_generated.h:156:16: error: ‘void* memset(void*, int, size_t)’ clearing an object of non-trivial type ‘struct MyGame::Example::NestedStruct’; use assignment or value-initialization instead [-Werror=class-memaccess]
  156 |     std::memset(d_, 0, sizeof(d_));
      |     ~~~~~~~~~~~^~~~~~~~~~~~~~~~~~~
/home/che7/Desktop/sourav/flatbuffers-1.12.0/tests/arrays_test_generated.h:66:40: note: ‘struct MyGame::Example::NestedStruct’ declared here
   66 | FLATBUFFERS_MANUALLY_ALIGNED_STRUCT(8) NestedStruct FLATBUFFERS_FINAL_CLASS {
      |                                        ^~~~~~~~~~~~
cc1plus: all warnings being treated as errors
make[2]: *** [CMakeFiles/flattests.dir/build.make:178: CMakeFiles/flattests.dir/tests/test.cpp.o] Error 1
make[1]: *** [CMakeFiles/Makefile2:175: CMakeFiles/flattests.dir/all] Error 2
make: *** [Makefile:166: all] Error 2

When searched online, I found that this issue is solved in later versions of flatbuffers.. Is a newer version of Flatbuffers supported for TI SDK? Or is there any other solution?