This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5K2E02: Which PCIe MSI system event should I use, and which interrupt, when they have the same description?

Part Number: AM5K2E02

Hi all

In Table 6-22 of SPRS864D, we have system events 30 (PCIE_0_INT4) and 32 (PCIE_0_INT6). But both of these are described as "PCIE MSI Interrupt". How do I choose which one to use? What's the difference?

Likewise Table 6-23 lists the CIC2 interrupts, but none of these correspond to PCIE0, so how can I work out which interrupt to use to provide a interrupt handler when a PCIE MSI event occurs? Which should I use?

thanks,