This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help



Good morning basically what I need is this program below could someone explain to me Funcines detailed so that I can make the necessary changes.

 

#include <stdio.h>
#include <c6x.h>
#include <ti/pspiom/cslr/cslr_gpio.h>
#include <ti/pspiom/cslr/cslr_syscfg_C6747.h>
#include <ti/pspiom/cslr/soc_C6747.h>
#include <ti/pspiom/cslr/cslr_psc_C6747.h>
#include <ti/pspiom/cslr/cslr_intc.h>

/*============================================================================*/
/*                             GLOBAL VARIABLES                               */
/*============================================================================*/

/* sys config registers overlay                                               */
CSL_SyscfgRegsOvly   sysRegs  = (CSL_SyscfgRegsOvly)(CSL_SYSCFG_0_REGS);
/* Psc register overlay                                                       */
CSL_PscRegsOvly      psc1Regs = (CSL_PscRegsOvly)(CSL_PSC_1_REGS);
/* Gpio register overlay                                                      */
CSL_GpioRegsOvly     gpioRegs = (CSL_GpioRegsOvly)(CSL_GPIO_0_REGS);
/* Interrupt Controller Register Overlay                                      */
CSL_IntcRegsOvly intcRegs = (CSL_IntcRegsOvly)CSL_INTC_0_REGS;

/*============================================================================*/
/*                        EXTERNAL FUNCTION PROTOTYPES                        */
/*============================================================================*/

extern void intcVectorTable(void);

static void delay(Uint32 count);


volatile Int32 status = 0;

#define GPIO0_EVENT    65
#define MAX_BLINK       4



void gpioExample(void)
{
    Uint32  ledBlinkCount = 0;
    volatile Uint32 temp = 0;
    volatile Uint32 pscTimeoutCount = 10240u;

    /* Key to be written to enable the pin mux registers to be written        */
    sysRegs->KICK0R = 0x83e70b13;
    sysRegs->KICK1R = 0x95A4F1E0;   

    /* mux between EMA_D8 and GPIO0_8 : enable GPIO0_8 (User Switch - "SW3-1")  */
    sysRegs->PINMUX14 = ( (CSL_SYSCFG_PINMUX14_PINMUX14_27_24_GPIO0_8) << \
                        (CSL_SYSCFG_PINMUX14_PINMUX14_27_24_SHIFT) );

    /* mux between EMA_D12 and GPIO0_12 : enable GPIO0_12 (User Led - "DS1")    */
    sysRegs->PINMUX15 = ( (CSL_SYSCFG_PINMUX15_PINMUX15_11_8_GPIO0_12) << \
                        (CSL_SYSCFG_PINMUX15_PINMUX15_11_8_SHIFT)  );

    /* lock the pinmux registers                                              */
    sysRegs->KICK0R = 0x00000000;
    sysRegs->KICK1R = 0x00000000;
   
  /* Bring the GPIO module out of sleep state                                 */
  /* Configure the GPIO Module to Enable state */
  psc1Regs->MDCTL[CSL_PSC_GPIO] =
                              ( (psc1Regs->MDCTL[CSL_PSC_GPIO] & 0xFFFFFFE0) |
                                 CSL_PSC_MDSTAT_STATE_ENABLE );
  /* Kick start the Enable Command */
  temp = psc1Regs->PTCMD;
  temp = ( (temp & CSL_PSC_PTCMD_GO0_MASK) |
           (CSL_PSC_PTCMD_GO0_SET << CSL_PSC_PTCMD_GO0_SHIFT) );
  psc1Regs->PTCMD |= temp;

  /*Wait for the power state transition to occur */
  while ( ((psc1Regs->PTSTAT & (CSL_PSC_PTSTAT_GOSTAT0_IN_TRANSITION)) != 0)
                     && (pscTimeoutCount>0) )
  {
      pscTimeoutCount--;
  }

  /* Check if PSC state transition timed out */
  if(pscTimeoutCount == 0)
  {
      printf("GPIO PSC transition to ON state timed out\n");
      return;
  }

  /* Wait for MODSTAT = ENABLE/DISABLE from LPSC */
  pscTimeoutCount = 10240u;
  while( ((psc1Regs->MDSTAT[CSL_PSC_GPIO] & (CSL_PSC_MDSTAT_STATE_MASK))
                != CSL_PSC_MDSTAT_STATE_ENABLE) && (pscTimeoutCount>0))
  {
      pscTimeoutCount--;
  }

  /* If timeout, the resource may not be functioning */
  if (0 == pscTimeoutCount)
  {
     printf("GPIO Module Enable timed out\n");
     return;
  }

  /* Configure GPIO0_12 (GPIO0_12_PIN) as an output */
  gpioRegs->BANK[0].DIR &= ~(CSL_GPIO_DIR_DIR_IN << CSL_GPIO_DIR_DIR12_SHIFT);

  /* Configure GPIO0_8 (GPIO0_8_PIN) as an input */
  temp = gpioRegs->BANK[0].DIR;
  temp = ( (temp & CSL_GPIO_DIR_DIR8_MASK) |
                      (CSL_GPIO_DIR_DIR_IN << CSL_GPIO_DIR_DIR8_SHIFT) );
  gpioRegs->BANK[0].DIR |= temp;


  /* Set Data high in SET_DATA register for GPIO(GPIO0_12_PIN).                *
   * This turns the LED off -see schematic                                    */
  temp = gpioRegs->BANK[0].SET_DATA;
  temp = ( (temp & CSL_GPIO_SET_DATA_SET12_MASK) |
            (CSL_GPIO_SET_DATA_SET_SET << CSL_GPIO_SET_DATA_SET12_SHIFT));
  gpioRegs->BANK[0].SET_DATA |= temp;

  /* Enable GPIO Bank interrupt for bank 0                                    */
  temp = gpioRegs->BINTEN;
  temp = ( (temp & CSL_GPIO_BINTEN_EN0_MASK) |
                    (CSL_GPIO_BINTEN_EN0_ENABLE << CSL_GPIO_BINTEN_EN0_SHIFT) );
  gpioRegs->BINTEN |= temp;

  /* Configure GPIO(GPIO0_8_PIN) to generate interrupt on rising edge         */
  temp = gpioRegs->BANK[0].SET_RIS_TRIG;
  temp = ( (temp & CSL_GPIO_SET_RIS_TRIG_SETRIS8_MASK) |
            (CSL_GPIO_SET_RIS_TRIG_SETRIS_ENABLE << CSL_GPIO_SET_RIS_TRIG_SETRIS8_SHIFT) );
  gpioRegs->BANK[0].SET_RIS_TRIG |= temp;

    /* map GPIO bank 0 event to cpu int4                                      */
    CSL_FINS(intcRegs->INTMUX1, INTC_INTMUX1_INTSEL4,GPIO0_EVENT);

    /* set ISTP to point to the vector table address                          */
    ISTP = (unsigned int)intcVectorTable;

    /* clear all interrupts, bits 4 thru 15                                   */
    ICR = 0xFFF0;

    /* enable the bits for non maskable interrupt and CPUINT4                 */
    IER = 0x12;

    /* enable interrupts, set GIE bit                                         */
    _enable_interrupts();

    printf("Waiting for GPIO Interrupt\n");

    while(0 == status)
    {
        printf("Waiting for user to configure SW3-1\n");
        delay(5000);
    }

     printf("GPIO Interrupt occured !\n");

    _disable_interrupts();

    while (ledBlinkCount++ < MAX_BLINK)
    {
        /* Make the GPIO pin (GPIO0_12_PIN) conected to the LED to low. *
         * This turns on the LED - see schematic         */
        temp = gpioRegs->BANK[0].CLR_DATA;
        temp = ( (temp & CSL_GPIO_CLR_DATA_CLR12_MASK) |
             (CSL_GPIO_CLR_DATA_CLR_CLR << CSL_GPIO_CLR_DATA_CLR12_SHIFT) );
        gpioRegs->BANK[0].CLR_DATA |= temp;

        delay(2000);

        /* Make the GPIO pin (GPIO0_12_PIN) conected to the LED to high *
         * This turns the off the LED - see schematic    */
        temp = gpioRegs->BANK[0].SET_DATA;
        temp = ( (temp & CSL_GPIO_SET_DATA_SET12_MASK) |
             (CSL_GPIO_SET_DATA_SET_SET << CSL_GPIO_SET_DATA_SET12_SHIFT) );
        gpioRegs->BANK[0].SET_DATA |= temp;


        delay(2000);
    }

    printf("End of GPIO sample application!\n");
}



void main (void)
{
   gpioExample();
}


interrupt void GPIO_input_isr()
{
    /* Let this be here now. I want to see the Heart beat :-) */
    status=1;
}


/*
 * \brief    Function to introduce a delay in to the program.
 *
 * \param    count [IN]  delay count to wait
 * \return   None
 *
 */
static void delay(Uint32 count)
{
    volatile Uint32 tempCount = 0;
    volatile Uint32 dummyCount = 0;

    for (tempCount = 0; tempCount < count; tempCount++)
    {
        for (dummyCount = 0; dummyCount < count; dummyCount++)
        {
            /* dummy loop to wait for some time  */
        }
    }
}

  •  

    Good Morning Leandro,

    This program is showing the usage of GPIO pins to toggle an LED & usage of Interrupt.

    Following is brief overview of the code

    1. In C6747, SoC pins are multiplexed. Initial few lines of code just selects the necessary functionality (GPIO) on a particular pin.

    2. Power State transition is done

    3. Interrupt & GPIO configuration

    4. interrupt  & LED togelling   

     

    An overview of CSLr is below

    1. CSL is used to access the bits of different registers of  the corresponding peripheral. (GPIO or any other like UART/I2C etc.)

    2. Following are the register overlay structures which are used here as Global Variables. 

        CSL_SYSCFG_0_REGS/ CSL_PSC_1_REGS/ CSL_GPIO_0_REGS/ CSL_INTC_0_REGS

    3. A register overlay structure is a structure having its element as all the registers of a peripheral.

    4. Thus for every peripheral there will be one register overlay structure And for every peripheral there will be one CSLr file.

    5. To access the specific bits of a register of a peripheral , Different Macros (MASK/SHIFT etc.) are defined in CSLr file.

     

    Now, Please have a look on the CSLr doc ( which i pointed in another thread) & then the CSLr file, then you will comfortable in making changes.

    Regards

    Prasad V. Joshi