Hi expert,
In the hardware checklist, below these pins need to be connected to GND/VDD through a resistor, but it not specify the resistor value. Can they connect directly without resistor? Thanks.

Best Regards,
Xingyu Zhu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
In the hardware checklist, below these pins need to be connected to GND/VDD through a resistor, but it not specify the resistor value. Can they connect directly without resistor? Thanks.

Best Regards,
Xingyu Zhu
Typically connecting directly is not a recommended design practice (especially for new designs), as an small hardware or software error can create power/GND short and damage the device. The pins cannot be left open/floating - as over time they can oscillate and/or drift into intermediate logic state and also damage the device. That is the reason for recommended pullup/down resistors.