I want to be able to boot LinuxOS from eMMC.
I tried to create an image file on Windows by following the Linux Appimage Generator Tool, but I got an error like below.
If you check the config file in the linuxAppimageGen folder, the path to the SDK is different from the actual path.
Compiler recognized path
C:/ti/ti-processor-sdk-linux-am62xx-evm-09.00.00.03
Actual SDK path
C:\ti\mcu_plus_sdk_am62x_09_00_00_19
Is this what I'm perceiving to be wrong?
If I'm wrong, please tell me the solution from the beginning.
thank you.