Hello All,
I am attempting to develop and application that will read data from a peripheral over the UPP bus and then transmit some data over the MII Ethernet port for the OMAPL138/C6748 EVM board.
I have both sub systems working from example code, but I am having a difficult time with the architecture side of things. I don't understand how to put both functions into one project. I started working with the socket examples Helloworld, client... but those projects spin off tasks to allow servers and the like. I don't need or want anything that sophisticated or resource hungry, I just want to spit out data to ta host computer every now and again to offload some DSP data. I did write a simple socket application which runs- but does 'nothing' since the sockets do not apparently inherently know how to get of the DSP. I looked a the MII example code supplied by Logic PD which was originally inteded to do a loopback test and that does work, but after modifying the code to just continuously send data- I find that it does not have any protocol associated and I can't seem to change the IP Address or the port for that matter- it's just EMAC transfers.
The UPP code looks pretty strainght forward I think- although I have not yet dug into it as I have been trying to get the Ethernet work right.
Any help on this would be great!
Mark