Part Number: PROCESSOR-SDK-AM62X
Hi, I would like to remove all qt5 recipes from tisdk-default-image, but it seems is not possible because some recipes are included into the arago distro file.
Any suggestions?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-AM62X
Hi, I would like to remove all qt5 recipes from tisdk-default-image, but it seems is not possible because some recipes are included into the arago distro file.
Any suggestions?
Thanks
Hi Mirko,
I would like to remove all qt5 recipes from tisdk-default-image
can you please try adding the below to conf/local.conf. When I do this a fair share of Qt-related libraries and other stuff seems to get eliminated. If you see something specific you want to remove beyond that, please let me know.
# Remove all Qt-related packages IMAGE_INSTALL:remove = "packagegroup-arago-tisdk-qte qtwebbrowser-examples qtwebengine-qmlplugins qtwebengine-examples" EXTRA_PACKAGES:remove:am62xx = "ti-apps-launcher"
Regards, Andreas
thanks but this not solve my problem
I would like to remove all qt5 recipes but seems is not possible
with the lines
IMAGE_INSTALL:remove = "packagegroup-arago-tisdk-qte qtwebbrowser-examples qtwebengine-qmlplugins qtwebengine-examples"
EXTRA_PACKAGES:remove:am62xx = "ti-apps-launcher"
there are always some qt packages in the image, from manifest:
qtbase aarch64 5.14.2+git0+3a6d8df521-r0.arago17.1
qtbase-conf am62xx_icore 1.0-r0.1
qtbase-plugins aarch64 5.14.2+git0+3a6d8df521-r0.arago17.1
qtbase-qmlplugins aarch64 5.14.2+git0+3a6d8df521-r0.arago17.1
qtdeclarative aarch64 5.14.2+git0+23a000f9a1-r0.tisdk1.1
qtdeclarative-plugins aarch64 5.14.2+git0+23a000f9a1-r0.tisdk1.1
qtdeclarative-qmlplugins aarch64 5.14.2+git0+23a000f9a1-r0.tisdk1.1
I think the problem is into the distro file arago.conf where qt5 is included, but if i remove all qt5 references in arago.conf the yocto build fails
Hi Mirko,
let me look into the distro file situation and see how to remove it from there. Please allow a couple of days for a response here.
Regards, Andreas
Mirko,
Any reason you want to use the tisdk-default-image as a base? If you want a minimal image I would recommend adding things to one of the core-image targets instead of trying to cutdown the arago images.
Regards,
Randolph
Any reason you want to use the tisdk-default-image as a base? If you want a minimal image I would recommend adding things to one of the core-image targets instead of trying to cutdown the arago images.
This is the way. Starting with a big yocto image and removing packages is much harder than starting with a smaller image and re-adding just the packages you want. Likely there are other packages included in the tisdk-default-image which have dependencies on qt and those are re-introducing qt to the final image.
Alternatively, copy the tisdk-default-image.bb into your own custom meta layer. Rename it to my-custom-image.bb. And then you can remove/add whatever packages you want.
I made a custom image, but the problem is the distro file arago.conf that contains some qt packages and if I try to remove the build crashes.
From what I see, the only references to qt in the arago.conf are PACKAGECONFIG lines those should have no effect if the qt packages aren't being included.
Try building core-image-minimal and see if arago.conf is still forcing qt to be included. I suspect it is not.
You might be able to generate a dependency tree to determine what is including qt. elinux.org/Bitbake_Cheat_Sheet
I just made the core-image-minimal, here is my manifest
alsa-conf aarch64 1.2.1.2-r0.1
alsa-ucm-conf all 1.2.1.2-r0.1
base-files am62xx_icore 3.0.14-r89.arago4.1
base-passwd aarch64 3.5.29-r0.1
bash aarch64 5.0-r0.arago0.1
busybox aarch64 1.31.1-r0.arago21.tisdk0.1
busybox-hwclock aarch64 1.31.1-r0.arago21.tisdk0.1
busybox-syslog aarch64 1.31.1-r0.arago21.tisdk0.1
busybox-udhcpc aarch64 1.31.1-r0.arago21.tisdk0.1
dbus-1 aarch64 1.12.24-r0.arago1.1
e2fsprogs-e2fsck aarch64 1.45.7-r0.1
init-ifupdown am62xx_icore 1.0-r7.arago1.tisdk2.1
initscripts-functions aarch64 1.0-r155.1
kbd aarch64 2.2.0-r0.1
kbd-consolefonts aarch64 2.2.0-r0.1
kbd-keymaps aarch64 2.2.0-r0.1
kernel-5.10.168-g999 am62xx_icore 5.10.168+git999-r0b.arago5.1
kernel-devicetree am62xx_icore 5.10.168+git999-r0b.arago5.1
kernel-image-5.10.168-g999 am62xx_icore 5.10.168+git999-r0b.arago5.1
kernel-image-fitimage-5.10.168-g999 am62xx_icore 5.10.168+git999-r0b.arago5.1
kernel-image-image-5.10.168-g999 am62xx_icore 5.10.168+git999-r0b.arago5.1
kernel-module-ipv6-5.10.168-g999 am62xx_icore 5.10.168+git999-r0b.arago5.1
kernel-module-pvrsrvkm-5.10.168-g999 am62xx_icore 1.15.6133109-r0b.11
kernel-module-sch-fq-codel-5.10.168-g999 am62xx_icore 5.10.168+git999-r0b.arago5.1
kmod aarch64 26-r0.1
ldconfig aarch64 2.30-r0.1
libacl1 aarch64 2.2.53-r0.1
libasound2 aarch64 1.2.1.2-r0.1
libattr1 aarch64 2.4.48-r0.1
libblkid1 aarch64 2.35.1-r0.1
libc6 aarch64 2.30-r0.1
libcap2 aarch64 2.32-r0.1
libcom-err2 aarch64 1.45.7-r0.1
libcrypto1.1 aarch64 1.1.1s-r0.1
libdbus-1-3 aarch64 1.12.24-r0.arago1.1
libdrm2 aarch64 2.4.101-r0.arago3.1
libe2p2 aarch64 1.45.7-r0.1
libevdev aarch64 1.8.0-r0.1
libevent-2.1-7 aarch64 2.1.11-r0.1
libexpat1 aarch64 2.2.9-r0.1
libext2fs2 aarch64 1.45.7-r0.1
libffi7 aarch64 3.3-r0.1
libfontconfig1 aarch64 2.13.1-r0.1
libfreetype6 aarch64 2.10.1-r0.arago0.1
libgcc-s1 aarch64 9.2.1-r0.1
libicudata66 aarch64 66.1-r0.1
libicui18n66 aarch64 66.1-r0.1
libicuuc66 aarch64 66.1-r0.1
libinput10 aarch64 1.15.2-r0.1
libjpeg62 aarch64 1:2.0.4-r0.1
libkmod2 aarch64 26-r0.1
liblzma5 aarch64 5.2.4-r0.1
libmount1 aarch64 2.35.1-r0.1
libnss-myhostname2 aarch64 1:244.5-r0.arago6.1
libpam aarch64 1.3.1-r0.1
libpam-runtime aarch64 1.3.1-r0.1
libpcre2-16-0 aarch64 10.34-r0.1
libpng16-16 aarch64 1.6.37-r0.1
libqt5webchannel-plugins aarch64 5.14.2+git0+d2c16a3e7e-r0.2
libqt5webchannel-qmlplugins aarch64 5.14.2+git0+d2c16a3e7e-r0.2
libqt5webchannel5 aarch64 5.14.2+git0+d2c16a3e7e-r0.2
libqt5webview-plugins aarch64 5.14.2+git0+9f479ce719-r0.1
libqt5webview-qmlplugins aarch64 5.14.2+git0+9f479ce719-r0.1
libqt5webview5 aarch64 5.14.2+git0+9f479ce719-r0.1
libsqlite3-0 aarch64 3:3.31.1-r0.1
libssl1.1 aarch64 1.1.1s-r0.1
libstdc++6 aarch64 9.2.1-r0.1
libsystemd0 aarch64 1:244.5-r0.arago6.1
libtinfo5 aarch64 6.2-r0.1
libudev1 aarch64 1:244.5-r0.arago6.1
libuuid1 aarch64 2.35.1-r0.1
libwebp aarch64 1.1.0-r0.1
libx11-compose-data aarch64 1.6.8-r0.0
libxkbcommon0 aarch64 0.10.0-r0.0
libz1 aarch64 1.2.11-r0.1
modutils-initscripts aarch64 1.0-r7.1
mtdev aarch64 1.1.6-r0.1
ncurses-terminfo-base aarch64 6.2-r0.1
netbase aarch64 2:6.1-r0.1
nspr aarch64 4.25-r0.1
nss aarch64 3.51.1-r0.1
openssl-conf aarch64 1.1.1s-r0.1
os-release all 1.0-r0.1
packagegroup-core-boot am62xx_icore 1.0-r17.1
pam-plugin-deny aarch64 1.3.1-r0.1
pam-plugin-env aarch64 1.3.1-r0.1
pam-plugin-faildelay aarch64 1.3.1-r0.1
pam-plugin-group aarch64 1.3.1-r0.1
pam-plugin-keyinit aarch64 1.3.1-r0.1
pam-plugin-lastlog aarch64 1.3.1-r0.1
pam-plugin-limits aarch64 1.3.1-r0.1
pam-plugin-loginuid aarch64 1.3.1-r0.1
pam-plugin-mail aarch64 1.3.1-r0.1
pam-plugin-motd aarch64 1.3.1-r0.1
pam-plugin-nologin aarch64 1.3.1-r0.1
pam-plugin-permit aarch64 1.3.1-r0.1
pam-plugin-rootok aarch64 1.3.1-r0.1
pam-plugin-securetty aarch64 1.3.1-r0.1
pam-plugin-shells aarch64 1.3.1-r0.1
pam-plugin-unix aarch64 1.3.1-r0.1
pam-plugin-warn aarch64 1.3.1-r0.1
qtbase aarch64 5.14.2+git0+3a6d8df521-r0.arago17.2
qtbase-conf am62xx_icore 1.0-r0.1
qtbase-plugins aarch64 5.14.2+git0+3a6d8df521-r0.arago17.2
qtbase-qmlplugins aarch64 5.14.2+git0+3a6d8df521-r0.arago17.2
qtdeclarative aarch64 5.14.2+git0+23a000f9a1-r0.tisdk1.2
qtdeclarative-plugins aarch64 5.14.2+git0+23a000f9a1-r0.tisdk1.2
qtdeclarative-qmlplugins aarch64 5.14.2+git0+23a000f9a1-r0.tisdk1.2
qtlocation aarch64 5.14.2+git0+feb604c326_d9577fdebe-r0.2
qtlocation-plugins aarch64 5.14.2+git0+feb604c326_d9577fdebe-r0.2
qtlocation-qmlplugins aarch64 5.14.2+git0+feb604c326_d9577fdebe-r0.2
qtwebengine aarch64 5.14.2+git0+35aa6c30f0_6c9be50c2d-r0.1
qtwebengine-plugins aarch64 5.14.2+git0+35aa6c30f0_6c9be50c2d-r0.1
qtwebengine-qmlplugins aarch64 5.14.2+git0+35aa6c30f0_6c9be50c2d-r0.1
run-postinsts all 1.0-r10.1
shadow aarch64 4.8.1-r0.1
shadow-base aarch64 4.8.1-r0.1
shadow-securetty am62xx_icore 4.6-r3.arago0.1
systemd aarch64 1:244.5-r0.arago6.1
systemd-compat-units aarch64 1.0-r29.1
systemd-conf am62xx_icore 244.3-r0.1
systemd-extra-utils aarch64 1:244.5-r0.arago6.1
systemd-serialgetty am62xx_icore 1.0-r5.1
systemd-vconsole-setup aarch64 1:244.5-r0.arago6.1
ti-img-rogue-driver am62xx_icore 1.15.6133109-r0b.11
ti-img-rogue-umlibs am62xx_icore 1.15.6133109-r2.1
ti-img-rogue-umlibs-plugins am62xx_icore 1.15.6133109-r2.1
tifs-lpm-stub am62xx_icore 08.03.02-r3.0.1
udev aarch64 1:244.5-r0.arago6.1
udev-hwdb aarch64 1:244.5-r0.arago6.1
update-alternatives-opkg aarch64 0.4.2-r0.1
update-rc.d all 0.8-r0.1
util-linux-agetty aarch64 2.35.1-r0.1
util-linux-fsck aarch64 2.35.1-r0.1
util-linux-mount aarch64 2.35.1-r0.1
util-linux-sulogin aarch64 2.35.1-r0.1
util-linux-umount aarch64 2.35.1-r0.1
volatile-binds all 1.0-r0.1
wayland aarch64 1.18.0-r0.1
xkeyboard-config aarch64 2.28-r0.0
as you can see there are many qt packages, below the list of the Qt library present in /usr/lib
./usr/lib/libQt5QuickWidgets.so.5.14.2
./usr/lib/libQt5QuickTest.so.5
./usr/lib/libQt5QuickWidgets.so.5.14
./usr/lib/libQt5WebEngine.so.5.14.2
./usr/lib/libQt5Concurrent.so.5.14.2
./usr/lib/libQt5PrintSupport.so.5.14.2
./usr/lib/libQt5Widgets.so.5.14
./usr/lib/libQt5DBus.so.5.14
./usr/lib/libQt5PositioningQuick.so.5
./usr/lib/libQt5OpenGL.so.5.14.2
./usr/lib/libQt5Gui.so.5.14
./usr/lib/libQt5QuickParticles.so.5.14.2
./usr/lib/libQt5QmlModels.so.5.14
./usr/lib/libQt5Positioning.so.5.14
./usr/lib/libQt5Gui.so.5.14.2
./usr/lib/libQt5Test.so.5.14
./usr/lib/libQt5Quick.so.5
./usr/lib/libQt5WebChannel.so.5.14.2
./usr/lib/libQt5WebView.so.5.14
./usr/lib/libQt5Xml.so.5.14.2
./usr/lib/libQt5Test.so.5
./usr/lib/libQt5EglFSDeviceIntegration.so.5.14.2
./usr/lib/libQt5Quick.so.5.14.2
./usr/lib/libQt5Location.so.5.14
./usr/lib/libQt5QmlModels.so.5.14.2
./usr/lib/libQt5WebView.so.5.14.2
./usr/lib/libQt5Core.so.5.14.2
./usr/lib/libQt5Core.so.5.14
./usr/lib/libQt5Xml.so.5.14
./usr/lib/libQt5EglFsKmsSupport.so.5
./usr/lib/libQt5WebEngineCore.so.5
./usr/lib/libQt5Core.so.5
./usr/lib/libQt5WebView.so.5
./usr/lib/libQt5WebEngine.so.5
./usr/lib/libQt5Positioning.so.5.14.2
./usr/lib/libQt5WebEngineCore.so.5.14
./usr/lib/libQt5Sql.so.5
./usr/lib/libQt5Qml.so.5.14.2
./usr/lib/libQt5WebChannel.so.5.14
./usr/lib/libQt5QuickShapes.so.5.14
./usr/lib/libQt5Network.so.5.14.2
./usr/lib/libQt5WebEngine.so.5.14
./usr/lib/libQt5Sql.so.5.14
./usr/lib/libQt5PositioningQuick.so.5.14
./usr/lib/libQt5Gui.so.5
./usr/lib/libQt5Quick.so.5.14
./usr/lib/libQt5QuickParticles.so.5.14
./usr/lib/libQt5QmlModels.so.5
./usr/lib/libQt5EglFsKmsSupport.so.5.14
./usr/lib/libQt5OpenGL.so.5
./usr/lib/libQt5Sql.so.5.14.2
./usr/lib/libQt5QuickTest.so.5.14.2
./usr/lib/libQt5EglFSDeviceIntegration.so.5
./usr/lib/libQt5WebEngineWidgets.so.5.14
./usr/lib/libQt5EglFSDeviceIntegration.so.5.14
./usr/lib/libQt5DBus.so.5.14.2
./usr/lib/libQt5QuickParticles.so.5
./usr/lib/libQt5Concurrent.so.5.14
./usr/lib/libQt5WebEngineWidgets.so.5.14.2
./usr/lib/libQt5OpenGL.so.5.14
./usr/lib/libQt5QmlWorkerScript.so.5
./usr/lib/libQt5Test.so.5.14.2
./usr/lib/libQt5WebEngineCore.so.5.14.2
./usr/lib/libQt5PrintSupport.so.5
./usr/lib/libQt5Location.so.5.14.2
./usr/lib/libQt5Network.so.5.14
./usr/lib/libQt5PositioningQuick.so.5.14.2
./usr/lib/libQt5Qml.so.5
./usr/lib/libQt5Widgets.so.5.14.2
./usr/lib/libQt5QuickShapes.so.5.14.2
./usr/lib/libQt5Widgets.so.5
./usr/lib/libQt5QmlWorkerScript.so.5.14
./usr/lib/libQt5QuickShapes.so.5
./usr/lib/libQt5QuickTest.so.5.14
./usr/lib/libQt5WebEngineWidgets.so.5
./usr/lib/libQt5QmlWorkerScript.so.5.14.2
./usr/lib/libQt5Positioning.so.5
./usr/lib/libQt5Xml.so.5
./usr/lib/libQt5QuickWidgets.so.5
./usr/lib/libQt5Location.so.5
./usr/lib/libQt5DBus.so.5
./usr/lib/libQt5EglFsKmsSupport.so.5.14.2
./usr/lib/libQt5Network.so.5
./usr/lib/libQt5PrintSupport.so.5.14
./usr/lib/libQt5Concurrent.so.5
./usr/lib/libQt5Qml.so.5.14
./usr/lib/libQt5WebChannel.so.5
Mirko,
Try removing meta-processor-sdk from your bblayers.conf. I'm not as familiar with what that layer is doing but I know nothing should be injecting dependencies in meta-arago and meta-ti.
Regards,
Randolph
Huh I don't get that. I also tried the sdk-09 config and that worked as well. bblayers does include meta-processor-sdk
./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-08.06.00-config.txt MACHINE=am62xx-evm bitbake core-image-minimal cat build/arago-tmp-external-arm-glibc/deploy/images/am62xx-evm/core-image-minimal-am62xx-evm.manifest base-files am62xx_evm 3.0.14-r89.arago4.0 base-passwd aarch64 3.5.29-r0.0 busybox aarch64 1.31.1-r0.arago21.tisdk0.0 busybox-hwclock aarch64 1.31.1-r0.arago21.tisdk0.0 busybox-syslog aarch64 1.31.1-r0.arago21.tisdk0.0 busybox-udhcpc aarch64 1.31.1-r0.arago21.tisdk0.0 dbus-1 aarch64 1.12.24-r0.arago1.0 e2fsprogs-e2fsck aarch64 1.45.7-r0.0 init-ifupdown am62xx_evm 1.0-r7.arago1.tisdk2.0 initscripts-functions aarch64 1.0-r155.0 kbd aarch64 2.2.0-r0.0 kbd-consolefonts aarch64 2.2.0-r0.0 kbd-keymaps aarch64 2.2.0-r0.0 kernel-5.10.168-g2c23e6c538 am62xx_evm 5.10.168+git0+2c23e6c538-r0b.arago5.0 kernel-devicetree am62xx_evm 5.10.168+git0+2c23e6c538-r0b.arago5.0 kernel-image-5.10.168-g2c23e6c538 am62xx_evm 5.10.168+git0+2c23e6c538-r0b.arago5.0 kernel-image-fitimage-5.10.168-g2c23e6c538 am62xx_evm 5.10.168+git0+2c23e6c538-r0b.arago5.0 kernel-image-image-5.10.168-g2c23e6c538 am62xx_evm 5.10.168+git0+2c23e6c538-r0b.arago5.0 kernel-module-ipv6-5.10.168-g2c23e6c538 am62xx_evm 5.10.168+git0+2c23e6c538-r0b.arago5.0 kernel-module-sch-fq-codel-5.10.168-g2c23e6c538 am62xx_evm 5.10.168+git0+2c23e6c538-r0b.arago5.0 kmod aarch64 26-r0.0 ldconfig aarch64 2.30-r0.0 libacl1 aarch64 2.2.53-r0.0 libattr1 aarch64 2.4.48-r0.0 libblkid1 aarch64 2.35.1-r0.0 libc6 aarch64 2.30-r0.0 libcap2 aarch64 2.32-r0.0 libcom-err2 aarch64 1.45.7-r0.0 libdbus-1-3 aarch64 1.12.24-r0.arago1.0 libe2p2 aarch64 1.45.7-r0.0 libexpat1 aarch64 2.2.9-r0.0 libext2fs2 aarch64 1.45.7-r0.0 libkmod2 aarch64 26-r0.0 liblzma5 aarch64 5.2.4-r0.0 libmount1 aarch64 2.35.1-r0.0 libnss-myhostname2 aarch64 1:244.5-r0.arago6.0 libpam aarch64 1.3.1-r0.0 libpam-runtime aarch64 1.3.1-r0.0 libsystemd0 aarch64 1:244.5-r0.arago6.0 libuuid1 aarch64 2.35.1-r0.0 libz1 aarch64 1.2.11-r0.0 modutils-initscripts aarch64 1.0-r7.0 netbase aarch64 2:6.1-r0.0 os-release all 1.0-r0.5 packagegroup-core-boot am62xx_evm 1.0-r17.0 pam-plugin-deny aarch64 1.3.1-r0.0 pam-plugin-env aarch64 1.3.1-r0.0 pam-plugin-faildelay aarch64 1.3.1-r0.0 pam-plugin-group aarch64 1.3.1-r0.0 pam-plugin-keyinit aarch64 1.3.1-r0.0 pam-plugin-lastlog aarch64 1.3.1-r0.0 pam-plugin-limits aarch64 1.3.1-r0.0 pam-plugin-loginuid aarch64 1.3.1-r0.0 pam-plugin-mail aarch64 1.3.1-r0.0 pam-plugin-motd aarch64 1.3.1-r0.0 pam-plugin-nologin aarch64 1.3.1-r0.0 pam-plugin-permit aarch64 1.3.1-r0.0 pam-plugin-rootok aarch64 1.3.1-r0.0 pam-plugin-securetty aarch64 1.3.1-r0.0 pam-plugin-shells aarch64 1.3.1-r0.0 pam-plugin-unix aarch64 1.3.1-r0.0 pam-plugin-warn aarch64 1.3.1-r0.0 run-postinsts all 1.0-r10.5 shadow aarch64 4.8.1-r0.0 shadow-base aarch64 4.8.1-r0.0 shadow-securetty am62xx_evm 4.6-r3.arago0.0 systemd aarch64 1:244.5-r0.arago6.0 systemd-compat-units aarch64 1.0-r29.0 systemd-conf am62xx_evm 244.3-r0.0 systemd-extra-utils aarch64 1:244.5-r0.arago6.0 systemd-serialgetty am62xx_evm 1.0-r5.0 systemd-vconsole-setup aarch64 1:244.5-r0.arago6.0 tifs-lpm-stub am62xx_evm 08.03.02-r3.0.0 udev aarch64 1:244.5-r0.arago6.0 udev-hwdb aarch64 1:244.5-r0.arago6.0 update-alternatives-opkg aarch64 0.4.2-r0.0 update-rc.d all 0.8-r0.5 util-linux-agetty aarch64 2.35.1-r0.0 util-linux-fsck aarch64 2.35.1-r0.0 util-linux-mount aarch64 2.35.1-r0.0 util-linux-sulogin aarch64 2.35.1-r0.0 util-linux-umount aarch64 2.35.1-r0.0 volatile-binds all 1.0-r0.5
Thanks Jonathan, Randolph, for chiming in here, much appreciated.
Mirko, another thing that might be helpful in such scenarios generally speaking is generating and inspecting the Yocto package/recipe dependency graph, see here: https://docs.yoctoproject.org/what-i-wish-id-known.html (specifically bullet 8: Know that you can generate a dependency graph and learn how to do it)
Regards, Andreas
Hi Andreas,
I create the graph, I removed meta-processor-sdk too but in core-image-minimal some qt packages are always included, so I suppose that with sdk-08.06.00 is not possible to remove some qt packages
Below the pn-buildlist contents made with the command bitbake -g core-image-minimal
core-image-minimal
quilt-native
patch-native
pseudo-native
linux-ti-staging
opkg-native
opkg-utils-native
xz-native
cross-localedef-native
qemuwrapper-cross
mklibs-native
prelink-native
makedevs-native
ldconfig-native
update-rc.d-native
bmap-tools-native
pigz-native
u-boot-ti-staging
tisdk-uenv
parted-native
gptfdisk-native
dosfstools-native
mtools-native
squashfs-tools-native
btrfs-tools-native
cdrtools-native
e2fsprogs-native
depmodwrapper-cross
syslinux-native
packagegroup-core-boot
qtwebview
qtwebengine
run-postinsts
tifs-lpm-stub
python3-setuptools-native
python3-six-native
python3-native
gnu-config-native
libtool-native
attr-native
automake-native
autoconf-native
pkgconfig-native
sqlite3-native
external-arm-toolchain
make-mod-scripts
rpm-native
dwarfsrcfiles-native
kmod-native
ncurses-native
dtc-native
u-boot-tools-native
bc-native
lzop-native
gmp-native
bison-native
libmpc-native
libarchive-native
libsolv-native
perl-native
gettext-minimal-native
qemu-native
elfutils-native
binutils-native
zlib-native
optee-os
trusted-firmware-a
ti-rtos-firmware
kern-tools-native
openssl-native
swig-native
flex-native
util-linux-native
texinfo-dummy-native
readline-native
popt-native
lz4-native
lzo-native
acl-native
nasm-native
qtbase-native
qtbase
libwebp
libevent
qtquickcontrols2
nss-native
alsa-lib
pulseaudio
pango
qtxmlpatterns
pciutils
libdrm
nss
openssl
ninja-native
qtlocation
cairo
gettext-native
qtwebchannel
gperf-native
fontconfig
icu
libcap
nspr-native
pixman
libpng
python-native
qtquickcontrols
libpng-native
qtdeclarative
systemd-systemctl-native
initscripts
update-rc.d
ncurses
zlib
unzip-native
libffi-native
gdbm-native
bzip2-native
autoconf-archive-native
libtirpc-native
libnsl2-native
debianutils-native
netbase
busybox
base-passwd
systemd-compat-units
base-files
shadow
modutils-initscripts
opkg-utils
systemd
init-ifupdown
m4-native
perl
xkeyboard-config
qtbase-conf
alsa-topology-conf
alsa-ucm-conf
alsa-utils-scripts
bash
bash-completion
alsa-utils
cryptodev-module
rsync-native
db-native
dbus-native
file-native
gtk-doc-native
mpfr-native
expat-native
cmake-native
glib-2.0-native
python3-pycryptodome-native
python3-pycryptodomex-native
python3-pyelftools-native
python3-cryptography-native
libpcre-native
libpcre2-native
libcap-ng-native
groff-native
freetype
libjpeg-turbo
libpcre2
ti-img-rogue-umlibs
wayland
libinput
libxkbcommon
dbus
libtool-cross
qtdeclarative-native
shadow-native
shadow-sysroot
ofono
sbc
libatomic-ops
glib-2.0
libxml-parser-perl-native
libtool
bluez5
libsndfile1
avahi
speexdsp
meson-native
gobject-introspection
gobject-introspection-native
harfbuzz
fribidi
kmod
libpthread-stubs
libpciaccess
sqlite3
nspr
cryptodev-linux
re2c-native
qtwebsockets
util-linux
expat
icu-native
libpam
attr
xz
acl
intltool-native
gdbm
db
libxslt-native
util-macros
libsamplerate0
shadow-securetty
python3
kbd
volatile-binds
systemd-conf
e2fsprogs
systemd-serialgetty
os-release
alsa-state
python3-asn1crypto-native
python3-idna-native
python3-cffi-native
ti-img-rogue-driver
libx11-compose-data
python3-dbus
python3-pygobject
mobile-broadband-provider-info
shared-mime-info
libnss-mdns
coreutils
curl-native
bzip2
libxml2
libffi
wayland-native
libevdev
mtdev
wayland-protocols
autoconf-archive
ell
libpcre
libical
readline
flac
libvorbis
libogg
libdaemon
libcap-ng
flex
cracklib
libxml2-native
libtirpc
libnsl2
python3-pycparser-native
python3-pycairo
shared-mime-info-native
itstool-native
gmp
ca-certificates
gawk
findutils
m4
cracklib-native
mc:k3r5-hs-fs:ti-sci-fw
mc:k3r5-hs-fs:quilt-native
mc:k3r5-hs-fs:patch-native
mc:k3r5-hs-fs:external-arm-toolchain
mc:k3r5-hs-fs:pseudo-native
mc:k3r5-hs-fs:rpm-native
mc:k3r5-hs-fs:dwarfsrcfiles-native
mc:k3r5-hs-fs:opkg-utils-native
mc:k3r5-hs-fs:xz-native
mc:k3r5-hs-fs:dtc-native
mc:k3r5-hs-fs:u-boot-tools-native
mc:k3r5-hs-fs:u-boot-ti-staging
mc:k3r5-hs-fs:openssl-native
mc:k3r5-hs-fs:python3-native
mc:k3r5-hs-fs:perl-native
mc:k3r5-hs-fs:gnu-config-native
mc:k3r5-hs-fs:libtool-native
mc:k3r5-hs-fs:attr-native
mc:k3r5-hs-fs:automake-native
mc:k3r5-hs-fs:autoconf-native
mc:k3r5-hs-fs:pkgconfig-native
mc:k3r5-hs-fs:rsync-native
mc:k3r5-hs-fs:bison-native
mc:k3r5-hs-fs:sqlite3-native
mc:k3r5-hs-fs:libarchive-native
mc:k3r5-hs-fs:popt-native
mc:k3r5-hs-fs:bzip2-native
mc:k3r5-hs-fs:db-native
mc:k3r5-hs-fs:elfutils-native
mc:k3r5-hs-fs:dbus-native
mc:k3r5-hs-fs:file-native
mc:k3r5-hs-fs:gettext-minimal-native
mc:k3r5-hs-fs:flex-native
mc:k3r5-hs-fs:ncurses-native
mc:k3r5-hs-fs:python3-setuptools-native
mc:k3r5-hs-fs:bc-native
mc:k3r5-hs-fs:kern-tools-native
mc:k3r5-hs-fs:lzop-native
mc:k3r5-hs-fs:swig-native
mc:k3r5-hs-fs:libffi-native
mc:k3r5-hs-fs:util-linux-native
mc:k3r5-hs-fs:gdbm-native
mc:k3r5-hs-fs:zlib-native
mc:k3r5-hs-fs:autoconf-archive-native
mc:k3r5-hs-fs:libtirpc-native
mc:k3r5-hs-fs:readline-native
mc:k3r5-hs-fs:libnsl2-native
mc:k3r5-hs-fs:m4-native
mc:k3r5-hs-fs:texinfo-dummy-native
mc:k3r5-hs-fs:acl-native
mc:k3r5-hs-fs:lzo-native
mc:k3r5-hs-fs:e2fsprogs-native
mc:k3r5-hs-fs:expat-native
mc:k3r5-hs-fs:unzip-native
mc:k3r5-hs-fs:libpcre-native
mc:k3r5-hs-fs:libpcre2-native
mc:k3r5-hs-fs:libcap-ng-native
mc:k3r5-gp:ti-sci-fw
mc:k3r5-gp:quilt-native
mc:k3r5-gp:patch-native
mc:k3r5-gp:external-arm-toolchain
mc:k3r5-gp:pseudo-native
mc:k3r5-gp:rpm-native
mc:k3r5-gp:dwarfsrcfiles-native
mc:k3r5-gp:opkg-utils-native
mc:k3r5-gp:xz-native
mc:k3r5-gp:dtc-native
mc:k3r5-gp:u-boot-tools-native
mc:k3r5-gp:u-boot-ti-staging
mc:k3r5-gp:openssl-native
mc:k3r5-gp:python3-native
mc:k3r5-gp:perl-native
mc:k3r5-gp:gnu-config-native
mc:k3r5-gp:libtool-native
mc:k3r5-gp:attr-native
mc:k3r5-gp:automake-native
mc:k3r5-gp:autoconf-native
mc:k3r5-gp:pkgconfig-native
mc:k3r5-gp:rsync-native
mc:k3r5-gp:bison-native
mc:k3r5-gp:sqlite3-native
mc:k3r5-gp:libarchive-native
mc:k3r5-gp:popt-native
mc:k3r5-gp:bzip2-native
mc:k3r5-gp:db-native
mc:k3r5-gp:elfutils-native
mc:k3r5-gp:dbus-native
mc:k3r5-gp:file-native
mc:k3r5-gp:gettext-minimal-native
mc:k3r5-gp:flex-native
mc:k3r5-gp:ncurses-native
mc:k3r5-gp:python3-setuptools-native
mc:k3r5-gp:bc-native
mc:k3r5-gp:kern-tools-native
mc:k3r5-gp:lzop-native
mc:k3r5-gp:swig-native
mc:k3r5-gp:libffi-native
mc:k3r5-gp:util-linux-native
mc:k3r5-gp:gdbm-native
mc:k3r5-gp:zlib-native
mc:k3r5-gp:autoconf-archive-native
mc:k3r5-gp:libtirpc-native
mc:k3r5-gp:readline-native
mc:k3r5-gp:libnsl2-native
mc:k3r5-gp:m4-native
mc:k3r5-gp:texinfo-dummy-native
mc:k3r5-gp:acl-native
mc:k3r5-gp:lzo-native
mc:k3r5-gp:e2fsprogs-native
mc:k3r5-gp:expat-native
mc:k3r5-gp:unzip-native
mc:k3r5-gp:libpcre-native
mc:k3r5-gp:libpcre2-native
mc:k3r5-gp:libcap-ng-native
mc:k3r5-hs-se:ti-sci-fw
mc:k3r5-hs-se:quilt-native
mc:k3r5-hs-se:patch-native
mc:k3r5-hs-se:external-arm-toolchain
mc:k3r5-hs-se:pseudo-native
mc:k3r5-hs-se:rpm-native
mc:k3r5-hs-se:dwarfsrcfiles-native
mc:k3r5-hs-se:opkg-utils-native
mc:k3r5-hs-se:xz-native
mc:k3r5-hs-se:dtc-native
mc:k3r5-hs-se:u-boot-tools-native
mc:k3r5-hs-se:u-boot-ti-staging
mc:k3r5-hs-se:openssl-native
mc:k3r5-hs-se:python3-native
mc:k3r5-hs-se:perl-native
mc:k3r5-hs-se:gnu-config-native
mc:k3r5-hs-se:libtool-native
mc:k3r5-hs-se:attr-native
mc:k3r5-hs-se:automake-native
mc:k3r5-hs-se:autoconf-native
mc:k3r5-hs-se:pkgconfig-native
mc:k3r5-hs-se:rsync-native
mc:k3r5-hs-se:bison-native
mc:k3r5-hs-se:sqlite3-native
mc:k3r5-hs-se:libarchive-native
mc:k3r5-hs-se:popt-native
mc:k3r5-hs-se:bzip2-native
mc:k3r5-hs-se:db-native
mc:k3r5-hs-se:elfutils-native
mc:k3r5-hs-se:dbus-native
mc:k3r5-hs-se:file-native
mc:k3r5-hs-se:gettext-minimal-native
mc:k3r5-hs-se:flex-native
mc:k3r5-hs-se:ncurses-native
mc:k3r5-hs-se:python3-setuptools-native
mc:k3r5-hs-se:bc-native
mc:k3r5-hs-se:kern-tools-native
mc:k3r5-hs-se:lzop-native
mc:k3r5-hs-se:swig-native
mc:k3r5-hs-se:libffi-native
mc:k3r5-hs-se:util-linux-native
mc:k3r5-hs-se:gdbm-native
mc:k3r5-hs-se:zlib-native
mc:k3r5-hs-se:autoconf-archive-native
mc:k3r5-hs-se:libtirpc-native
mc:k3r5-hs-se:readline-native
mc:k3r5-hs-se:libnsl2-native
mc:k3r5-hs-se:m4-native
mc:k3r5-hs-se:texinfo-dummy-native
mc:k3r5-hs-se:acl-native
mc:k3r5-hs-se:lzo-native
mc:k3r5-hs-se:e2fsprogs-native
mc:k3r5-hs-se:expat-native
mc:k3r5-hs-se:unzip-native
mc:k3r5-hs-se:libpcre-native
mc:k3r5-hs-se:libpcre2-native
mc:k3r5-hs-se:libcap-ng-native
What machine are you building for? See my post above, I tested the 08.06 sdk and saw no qt packages built. You might want to try a clean build because I cannot reproduce what your showing so it looks like its something on your side.