This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is there connections between the power rails inside the DM8168?



We are bringing up a prototype board with the DM8168 and confirming the power sequence and timing.  We noticed the 1.0V AVS rail seems to come through on the 1.5V ALT rail, or one of the 1.5V rails.  We also observed this voltage "mirroring" on the EVM board from Spectrum Digital, so we do not think this is isolated to this particular board and layout.  Anyone else observe this behavior?

Thanks,

Paul