This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VE-Q1: TIDL: onnx issue

Part Number: TDA4VE-Q1


Hi, Expert, 

onnx 1.7.0 didn't work on my side. Can I upgrade to 1.14.0 ? pls help to share your comments. 

Requirement already satisfied: protobuf in /home/fredy/.local/lib/python3.10/site-packages (from onnx==1.7.0) (3.20.3)
Requirement already satisfied: numpy in /home/fredy/.local/lib/python3.10/site-packages (from onnx==1.7.0) (1.23.0)
Requirement already satisfied: six in /usr/lib/python3/dist-packages (from onnx==1.7.0) (1.16.0)
Requirement already satisfied: typing-extensions>=3.6.2.1 in /home/fredy/.local/lib/python3.10/site-packages (from onnx==1.7.0) (4.6.3)
Building wheels for collected packages: onnx
  Building wheel for onnx (pyproject.toml) ... error
  error: subprocess-exited-with-error
  
  × Building wheel for onnx (pyproject.toml) did not run successfully.
  │ exit code: 1
  ╰─> [94 lines of output]
      fatal: not a git repository (or any of the parent directories): .git
      /tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/dist.py:744: SetuptoolsDeprecationWarning: Invalid dash-separated options
      !!
      
              ********************************************************************************
              Usage of dash-separated 'license-file' will not be supported in future
              versions. Please use the underscore name 'license_file' instead.
      
              By 2023-Sep-26, you need to update your project and remove deprecated calls
              or your builds will no longer be supported.
      
              See https://setuptools.pypa.io/en/latest/userguide/declarative_config.html for details.
              ********************************************************************************
      
      !!
        opt = self.warn_dash_deprecation(opt, section)
      /tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/config/setupcfg.py:293: _DeprecatedConfig: Deprecated config in `setup.cfg`
      !!
      
              ********************************************************************************
              The license_file parameter is deprecated, use license_files instead.
      
              By 2023-Oct-30, you need to update your project and remove deprecated calls
              or your builds will no longer be supported.
      
              See https://setuptools.pypa.io/en/latest/userguide/declarative_config.html for details.
              ********************************************************************************
      
      !!
        parsed = self.parsers.get(option_name, lambda x: x)(value)
      running bdist_wheel
      running build
      running build_py
      running create_version
      running cmake_build
      Traceback (most recent call last):
        File "/home/fredy/.local/bin/cmake", line 5, in <module>
          from cmake import cmake
      ModuleNotFoundError: No module named 'cmake'
      Traceback (most recent call last):
        File "/home/fredy/.local/lib/python3.10/site-packages/pip/_vendor/pyproject_hooks/_in_process/_in_process.py", line 353, in <module>
          main()
        File "/home/fredy/.local/lib/python3.10/site-packages/pip/_vendor/pyproject_hooks/_in_process/_in_process.py", line 335, in main
          json_out['return_val'] = hook(**hook_input['kwargs'])
        File "/home/fredy/.local/lib/python3.10/site-packages/pip/_vendor/pyproject_hooks/_in_process/_in_process.py", line 251, in build_wheel
          return _build_backend().build_wheel(wheel_directory, config_settings,
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/build_meta.py", line 434, in build_wheel
          return self._build_with_temp_dir(
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/build_meta.py", line 419, in _build_with_temp_dir
          self.run_setup()
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/build_meta.py", line 507, in run_setup
          super(_BuildMetaLegacyBackend, self).run_setup(setup_script=setup_script)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/build_meta.py", line 341, in run_setup
          exec(code, locals())
        File "<string>", line 321, in <module>
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/__init__.py", line 107, in setup
          return distutils.core.setup(**attrs)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/core.py", line 185, in setup
          return run_commands(dist)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/core.py", line 201, in run_commands
          dist.run_commands()
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/dist.py", line 969, in run_commands
          self.run_command(cmd)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/dist.py", line 1233, in run_command
          super().run_command(command)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/dist.py", line 988, in run_command
          cmd_obj.run()
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/wheel/bdist_wheel.py", line 364, in run
          self.run_command("build")
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/cmd.py", line 318, in run_command
          self.distribution.run_command(command)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/dist.py", line 1233, in run_command
          super().run_command(command)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/dist.py", line 988, in run_command
          cmd_obj.run()
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/command/build.py", line 131, in run
          self.run_command(cmd_name)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/cmd.py", line 318, in run_command
          self.distribution.run_command(command)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/dist.py", line 1233, in run_command
          super().run_command(command)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/dist.py", line 988, in run_command
          cmd_obj.run()
        File "<string>", line 217, in run
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/cmd.py", line 318, in run_command
          self.distribution.run_command(command)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/dist.py", line 1233, in run_command
          super().run_command(command)
        File "/tmp/pip-build-env-d6c4qibr/overlay/local/lib/python3.10/dist-packages/setuptools/_distutils/dist.py", line 988, in run_command
          cmd_obj.run()
        File "<string>", line 203, in run
        File "/usr/lib/python3.10/subprocess.py", line 369, in check_call
          raise CalledProcessError(retcode, cmd)
      subprocess.CalledProcessError: Command '['/home/fredy/.local/bin/cmake', '-DPYTHON_INCLUDE_DIR=/usr/include/python3.10', '-DPYTHON_EXECUTABLE=/usr/bin/python3', '-DBUILD_ONNX_PYTHON=ON', '-DCMAKE_EXPORT_COMPILE_COMMANDS=ON', '-DONNX_NAMESPACE=onnx', '-DPY_EXT_SUFFIX=.cpython-310-x86_64-linux-gnu.so', '-DCMAKE_BUILD_TYPE=Release', '-DONNX_ML=1', '/tmp/pip-install-s0lf2ci3/onnx_5ff923c3665f473e8b9eb629e1e9089c']' returned non-zero exit status 1.
      [end of output]
  
  note: This error originates from a subprocess, and is likely not a problem with pip.
  ERROR: Failed building wheel for onnx
Failed to build onnx
ERROR: Could not build wheels for onnx, which is required to install pyproject.toml-based projects

Regards,

Fredy Zhang