This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: How to enable UART2 for serial port loopback test

Part Number: TDA4VM

Hello,

Hello, we already know that USB contains UART0 and UART1. The internal UART information can be sent and received through the official serialcheck. After consulting the data, the TX and RX of UART2 are located at pins 8 and 10 in the 40 pin header, but We modified the device tree and found that UART2 still cannot be enabled. Looking at the source code, we found that UART2 does not enable dma mode or interrupt. How to enable UART2 for serial communication? And can you give the code to enable the interrputs or the address of the dma available for UART2?Looking forward to your reply, thank you.

Regards,

Gary